how to enable the BT.1120 in imx6 linux BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to enable the BT.1120 in imx6 linux BSP

1,711件の閲覧回数
huangjacky
Contributor III

Dear All:

I got the imx6 HW platform with ADV7441, the ADV7441 is HDMI ---> CSI encoder, support bt1120 interface.

Now I have confirm the i2c connect with ADV7441 is work.

I found the imx6 linux BSP is only support 8 or 10 bits bt.656, but found nothing with bt.1120.

refence the link: https://community.freescale.com/thread/303792

Qiang LiEmployee

For iMX6 BSP, the BT1120 16bits mode was not ready yet, we don't have the real hardware to enable it. Maybe you need reference to the iMX53 patch to support it.

I wanna know how to enable the bt.1120 function in imx6 linux BSP?

Thanks Advance!

ラベル(3)
タグ(4)
2 返答(返信)

705件の閲覧回数
YixingKong
Senior Contributor IV

Hi Jacky, please click Correct Answer/Helpful Answer, if your question had been answered.

Thanks,

Yixing

0 件の賞賛

705件の閲覧回数
max_tsai
NXP Employee
NXP Employee

hi Jacky,

Please refer to https://community.freescale.com/docs/DOC-94019

-Max