how to enable lvds split mode for uboot-2015.04

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to enable lvds split mode for uboot-2015.04

840件の閲覧回数
fulinux
Contributor IV


Hi,

i have tested uboot-2009.08 logo, but it not good(look at this thread uboot logo color is not normal ) i want to test uboot-2015.05 what it is fsl new version. for my lcd panel is 1920x1080 pix, it should use split mode, i don't know how to modify uboot-2015.04 to enable split mode, is it doesn't matter with this thread Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L...  right ?

ラベル(1)
タグ(2)
0 件の賞賛
1 返信

375件の閲覧回数
b36401
NXP Employee
NXP Employee

You can try to configure it manually with updating LDB_CTRL register.

Please refer to 39.6.1 "LDB Control Register" chapter of i.MX 6Dual/6Quad Applications Processor Reference Manual.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛