I have attached a patch that shows implementation for slave mode. This was done for MX51, but should be similar for MX53. Hope this helps.
Hi Sanjeev,
The patch that was attached is to make the MX6 behave as a SPI slave device. By default, the driver provided in the BSP configures the MX6 SPI to be master.
So if you have a SPI slave device with MX6 as SPI master, then you do not need this patch.
Best regards,
-Mahesh
HI maheshmahadevan-r9aadq, are the patches to make the MX6 behave as SPI slave for the i.MX6 platform SDK?
Leo
Thanks Mahesh,
Are you referring to same patch attached by you need to port on kernel i
have been using for imx6 platform.I there any limitation if device is
working in slave mode?
Regards
Sanju
On Sat, May 11, 2013 at 1:56 AM, Mahesh Mahadevan <