how to configure JTAG as JTAG instead of SAI in iMX6ULL dts file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to configure JTAG as JTAG instead of SAI in iMX6ULL dts file

1,130 Views
devika_ramesh
Contributor I

how to cnfigure JTAG as JTAG instead of SAI in IMX6ULL dts file

Tags (1)
0 Kudos
Reply
3 Replies

1,069 Views
igorpadykov
NXP Employee
NXP Employee

Hi devika

seems one can remove or comment sai2 signals from dts file

imx6ull-14x14-evk.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

also may be useful:  https://community.nxp.com/thread/262294 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,069 Views
devika_ramesh
Contributor I

Could you please share the code snippet on how to add the node for JTAG

signals in dts file

0 Kudos
Reply

1,069 Views
devika_ramesh
Contributor I

Hi Igor

Could you please share the code snippet on how to add the node for JTAG signals in dts file

0 Kudos
Reply