how to configure 8GDDR for IMX8QM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to configure 8GDDR for IMX8QM

482件の閲覧回数
coindu
Contributor IV

Hi NXP team,

        The IMX8QM-evk board is 6GDDR, and now we customized a board to use 8G ddr. can you help me to configure it.

         The bsp is base on L4.19.35..

         Now I have been generated scfw_tcm.bin with 8G ddr config file(imx8qm_dcd_1.6GHz.cfg).and modify u-boot include/configs/xxxx.h

#define CONFIG_SYS_SDRAM_BASE 0x80000000
#define PHYS_SDRAM_1 0x80000000
#define PHYS_SDRAM_2 0x880000000
#define PHYS_SDRAM_1_SIZE 0x100000000 /* 4 GB */
#define PHYS_SDRAM_2_SIZE 0x100000000 /* 4 GB */

 

         But the imx-atf will use 0xfe00 0000 address to load bin. When I change plat/imx/imx8qm/include/platform_def.h 

        #define BL32_BASE 0xfe000000 -> 0x17e000000,

imx-boot iMX8QM/soc.mak

        0xFE000000 -> 0x17e000000 , It will stuck at

 U-Boot SPL 2019.04-4.19.35-1.1.0+g3987e27 (Jan 07 2023 - 03:18:57 +0000)
Normal Boot
Trying to boot from MMC2_2
Load image from MMC/SD 0x67000
U

      Is there any document can be provided  about how to support large memory

0 件の賞賛
2 返答(返信)

474件の閲覧回数
coindu
Contributor IV

It is seem that,u-boot get ram start_address and end_size from scfw. The scfw should be modify something about it.

[7] vir = 0x80020000 phys = 0x80020000 size = 0x7dfe0000 attrs = 0x210
[8] vir = 0x100000000 phys = 0x100000000 size = 0x0 attrs = 0x210

but I do not know where to modify it. 

0 件の賞賛

443件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you use your company email , so that you can got Higher privilege support?

0 件の賞賛