how to compile fw_printenv / fw_saveenv with fsl-community-bsp?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to compile fw_printenv / fw_saveenv with fsl-community-bsp?

1,502 次查看
pavelkopylov
Contributor III

Recipe "u-boot-fw-utils" compilation failed.

ERROR: Function failed: do_compile (log file is located at /home/fsl-community-bsp/build/tmp/work/cgtqmx6-poky-linux-gnueabi/u-boot-fw-utils/v2013.07+gitAUTOINC+62c175fbb8-r0/temp/log.do_compile.18430)

ERROR: Logfile of failure stored in: /home/fsl-community-bsp/build/tmp/work/cgtqmx6-poky-linux-gnueabi/u-boot-fw-utils/v2013.07+gitAUTOINC+62c175fbb8-r0/temp/log.do_compile.18430

Log data follows:

| DEBUG: Executing shell function do_compile

| NOTE: make -j 2 HOSTCC=arm-poky-linux-gnueabi-gcc  -march=armv7-a -mthumb-interwork -mfloat-abi=hard -mfpu=neon -mtune=cortex-a9 --sysroot=/home/fsl-community-bsp/build/tmp/sysroots/cgtqmx6 HOSTSTRIP=true cgtqmx6_config

| make: *** No rule to make target `cgtqmx6_config'.  Stop.

| make: *** [cgtqmx6_config] Error 1

| ERROR: oe_runmake failed

| WARNING: exit code 1 from a shell command.

| ERROR: Function failed: do_compile (log file is located at /home/fsl-community-bsp/build/tmp/work/cgtqmx6-poky-linux-gnueabi/u-boot-fw-utils/v2013.07+gitAUTOINC+62c175fbb8-r0/temp/log.do_compile.18430)

ERROR: Task 6 (/home/fsl-community-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot-fw-utils_2013.07.bb, do_compile) failed with exit code '1'

标签 (1)
0 项奖励
回复
2 回复数

791 次查看
allanmatthew
Contributor IV

Pavel-

Were you able to resolve this issue? I'm running into the same problem.

-Allan

0 项奖励
回复

791 次查看
allanmatthew
Contributor IV

Figured it out.  Its necessary to use your own u-boot repo, not the default.

0 项奖励
回复