hi .. i have raw format image which is not showing up on imx53.. can u tell me whish all format can run on imx53.. actually i tried making liveusb image but it say this format is not supported my arm7hl architechture... how can i cnfigure kernel
You should have iMX53 QSB (quick start board).
My suggestion for you is: start booting up a pure linux image, just like Freescale releases for QSB. When you understand what binaries you need, and how to copy them to SDCard, you can choose which one you will use.
I haven´t worked with Meego images, but I believe you will need to modify (someway) they kernel source code.
Take this document package: https://www.freescale.com/webapp/Download?colCode=IMX53_QSB_1101_LINUXDOCS_BUNDLE&location=null&fpsp...
untar and open it. Go first on doc\mx5\i.MX53_START_Linux_BSP_UserGuide.pdf
To take source code, http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab#
Once you are able to load a pre-built image you can start working on Meego source code
http://wiki.meego.com/Image_Creation
http://wiki.meego.com/Image_Creation_For_Beginners
http://wiki.meego.com/ARM/Creating_ARM_Image_using_Meego_Image_Creator
I have created image and donno how to boot it on i.mx53... do i need any other thing like extra bootloader as i think bootloader is a part of image only... Lemme know what is going wrong
Daiane Angolini said:
Are you using which bootloader?
How did you configured kernel?
Please, share the procedure to create SDCard.
Can you share me the link you´ve been using to get started with meego?
What's your hardware board? Generally there should be some switches on the boards to let you be able to configure boot mode. You should find how to jump the switches for booting from a SD card on that board.
Are you using which bootloader?
How did you configured kernel?
Please, share the procedure to create SDCard.
Can you share me the link you´ve been using to get started with meego?