how to boot meego image on I.mx53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to boot meego image on I.mx53

1,497 Views
WasimShaikh_ng
Contributor I
Hi i m using i.mx53. i want to boot meego image which i have created on i.mx53. But when i put that image on SDCARD and S/w on the i.mx53 its not showing up anything..Can anyone tell me whr m i going wrong.. i m new to this environment. I have created meego image with MIC2 and my image size is approx 1,7Gb... How can i boot that image.. is thr anything more i need..
Tags (1)
0 Kudos
Reply
7 Replies

1,312 Views
daiane_angolini
NXP Employee
NXP Employee
Have you tried to get help from meego mail list?http://lists.meego.com/listinfo/meego-porting I´m sure they are the best source of information regarding meego. Sorry for not helping you on this task. I really don´t know meego architecture.
0 Kudos
Reply

1,312 Views
WasimShaikh_ng
Contributor I

hi .. i have raw format image which is not showing up on imx53.. can u tell me whish all format can run on imx53.. actually i tried making liveusb image but it say this format is not supported my arm7hl architechture... how can i cnfigure kernel

0 Kudos
Reply

1,312 Views
daiane_angolini
NXP Employee
NXP Employee

You should have iMX53 QSB (quick start board).

 

My suggestion for you is: start booting up a pure linux image, just like Freescale releases for QSB. When you understand what binaries you need, and how to copy them to SDCard, you can choose which one you will use.

 

I haven´t worked with Meego images, but I believe you will need to modify (someway) they kernel source code.

 

Take this document package: https://www.freescale.com/webapp/Download?colCode=IMX53_QSB_1101_LINUXDOCS_BUNDLE&location=null&fpsp...

 

untar and open it. Go first on doc\mx5\i.MX53_START_Linux_BSP_UserGuide.pdf

 

To take source code, http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab#

 

Once you are able to load a pre-built image you can start working on Meego source code

0 Kudos
Reply

1,312 Views
WasimShaikh_ng
Contributor I

http://wiki.meego.com/Image_Creation

http://wiki.meego.com/Image_Creation_For_Beginners

http://wiki.meego.com/ARM/Creating_ARM_Image_using_Meego_Image_Creator

 

 

I have created image and donno how to boot it on i.mx53... do i need any other thing like extra bootloader as i think bootloader is a part of image only... Lemme know what is going wrong

 


Daiane Angolini said:

Are you using which bootloader?

How did you configured kernel?

Please, share the procedure to create SDCard.

 

Can you share me the link you´ve been using to get started with meego?

0 Kudos
Reply

1,312 Views
WasimShaikh_ng
Contributor I
Its I.mx 53... i just have image and i guess bootloader is part of image only... i donno...what switch u r talking abt... thr is only power on switch on it..... is it right that bootloader is part of image??? and if not pls lemme know how to boot image and what all other software i need to run it...

Shenwei Wang said:
What's your hardware board? Generally there should be some switches on the boards to let you be able to configure boot mode. You should find how to jump the switches for booting from a SD card on that board.
0 Kudos
Reply

1,312 Views
ShenweiWang
NXP Employee
NXP Employee
What's your hardware board? Generally there should be some switches on the boards to let you be able to configure boot mode. You should find how to jump the switches for booting from a SD card on that board.
0 Kudos
Reply

1,312 Views
daiane_angolini
NXP Employee
NXP Employee

Are you using which bootloader?

How did you configured kernel?

Please, share the procedure to create SDCard.

 

Can you share me the link you´ve been using to get started with meego?

0 Kudos
Reply