I have a MIMXRT1050-EVK board.I downloaded gpio example code and flash through IAR having (MIMXRT1052xxxxx_sdram. icf ) file using I-Jet to EVK Board keeping SW7 off on on off, pins as shown in Data Sheet, and flashing successfully and the led blinking.
when I power off and power on the earlier code ( blink Led ) is not working.
1. Is that code is running from sram if so I want run the code from hyper flash how can I ..? ( The same code has to run even when I power off).
Hi prashanth,
Attached you can find a document showing the steps to program Hyper flash.
Please note that it can require double-headed USB cable for higher current capability on some laptops. Lower current capability can cause incorrect power sequence (see requirement for power sequence in device datasheet) during RT power up and this can lead into the boot failure. Another option is to move J1 to 1-2 and supply power through the barrel connector instead.
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Carlos_Musich,
1. As you said In the above mail I have gone through PDF file, I have following debug files in my Hello world program
1. sdram_debug
2. flexspi_nor_debug
3. sdram_txt_debug
4. debug
there is no hyper_debug in above options.and I did't find any MIMXRT1052xxx6A_hyper.icf in the downloaded programs.
2. When I select flexspi_nor_debug, It is showing following error.
" Verification Error 0x60002001 : mem = 0x80, file = 0x00"
3, When I try modify icf file with configurations as you said PDF file it is showing as above same error
" Verification Error 0x60002001 : mem = 0x80, file = 0x00"
Note : The following things are doing in below conditions
1. I flashing through I-Jet i-link Debugger.
2. Keeping SW7 switch as 0 11 0 ( off on on off) as said in Data sheet for ( Hyper Flash)
3. For time being I added those 0 ohm resistors at following loacations (R153, R154, R155, R156, R157, R158)
Please help me where I am doing mistake ASAP.
Hi prashanthchary, the flexspi_nor_debug target is configured to link code to the FlexSPI region for Hyperflash (or QSPI) targets.
The issue you are seeing with Verify errors may be related to the Reset type used by the debugger. It seems you are using I-Jet. I would suggest modifying the Reset type in the debug options to "Core" type. Also, make sure the interface is set to SWD, not JTAG.
Project > Options > I-jet/JTAGjet > Setup
Project > Options > I-jet/JTAGjet > Interface
Currently, the hello_world project for IAR does not include the IVT, boot data needed to create a bootable image to run out of reset. You can use the drag/drop feature described in the HyperFlashprog_MXRT1050.pdf to create and program an image into the Hyperflash that will execute after a power off/on. (Just note, it's using the flexspi_nor_debug instead of the hyper_debug. It looks like that guide is out of date). Here is some additional information about the drag/drop:
i.MX RT1050 CMSIS-DAP drag-and-drop programming.
Also, you will need to generate a .bin output from the compile step which can be specified in
Project > Options > Output Converter
Check the "Generate additional Output"
Select "Raw Binary"
Hi Prashanth,
1. Make sure that you have downloaded the latest SDK available via Welcome | MCUXpresso SDK Builder.
2. Also, it will be better if you don't connect those resistors. Those resistors are needed if you want to boot from the QSPI flash.
Hi, I have the same problem.
I want to debug from the Hyperflash.
I am using IAR EWARM 8.20.
I already downloaded the latest mimxrt1050 SDK, keeping SW7 switch on EVK board as 0 11 0 ( off on on off).
When I select flexspi_nor_debug, before debugging start it creates following error:
" Verification Error at 0x60002001 : mem = 0x80, file = 0x00"
" Download completed but verification failed."
Please help