hdmi 1080p60 pixel clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

hdmi 1080p60 pixel clock

2,012件の閲覧回数
endl
Contributor II

Hello

I'm testing 1080p60 rendering on hdmi.

For 1080p60 the pixel clock must be set to 148.5MHz

From "iMX 6Series Plarform SDK v1.1.0" I found this code

   switch (pclk) {    // pixel clock

        case 74250000:

        case 148500000:

            //clk output from 540M PFD1 of PLL3 

            HW_CCM_CHSCCDR.B.IPU1_DI0_CLK_SEL = 0;  // derive clock from divided pre-muxed ipu1 di0 clock

            HW_CCM_CHSCCDR.B.IPU1_DI0_PODF = 5; // div by 6

            HW_CCM_CHSCCDR.B.IPU1_DI0_PRE_CLK_SEL = 5;  // derive clock from 540M PFD

            //config PFD1 of PLL3 to be 445MHz 

            BW_CCM_ANALOG_PFD_480_PFD1_FRAC(0x13);

            break;

        default:

            printf("the hdmi pixel clock is not supported!\n");

    }

1.png

The resulting clock is 445MHz / 6 = 74.2MHz for 1080p60 and 720p60.

Is that right ??? Why ipu1_di0 clock divider is not set to 3 for 1080p60 ?

ラベル(2)
0 件の賞賛
返信
1 返信

822件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Vadim

seems SDK was not tested with 1080p60 so there are no

codes for it. You can add suitable coefficient yourself and test.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信