I used gstreamer-imx on i.MX6DL before. But I can't use it on i.MX8X.
(The reason for using i.MX8X is supported "Automotive" same as the i.MX6DL.)
I cannot find i.MX8X in "Currently tested" on the page, https://github.com/Freescale/gstreamer-imx.
Also, the imx-yocto-L5.4.70_2.3.0 doesn't have the gstreamer-imx element.
Is it planned to support it? If it does, when would it be available?
Solved! Go to Solution.
Hi. @joanxie
Thank you for giving the information.
Although that page doesn't write i.MX8X in the "Currently tested", I found out that i.MX8X actually supports the gstreamer-imx.
imx8x still supports gstreamer 1.0, what do you need ? you need to how to use it on imx8x or you need source code?
Hi. @joanxie
I need the gstreamer-imx that works on imx8x.
for 5.4.70, maybe you can refer to the link as below:
"https://source.codeaurora.org/external/imx/imx-gst1.0-plugin/tree/?h=MM_04.05.07_2011_L5.4.70"
Hi. @joanxie
Thank you for giving the information.
Although that page doesn't write i.MX8X in the "Currently tested", I found out that i.MX8X actually supports the gstreamer-imx.