gstreamer(0.10) issue for imx53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gstreamer(0.10) issue for imx53

1,023 Views
kravik
Contributor IV

I am getting error while running gstreamer using VPU. I am working on IMX53 based customized board.

#gst-launch filesrc location=Avengers.mp4 typefind=true ! aiurdemux ! queue max-size-time=0 ! mfw_vpudecoder ! mfw_v4lsink

(gst-plugin-scanner:786): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_mp3dec.so': lib_mp3_dec_army

(gst-plugin-scanner:786): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_aacdec.so': lib_aac_dec_army

(gst-plugin-scanner:786): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_vorbisdec.so': lib_oggvorbiy

(gst-plugin-scanner:786): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_aacplusdec.so': lib_aac_decy

(gst-plugin-scanner:786): GStreamer-CRITICAL **: gst_element_class_add_pad_template: assertion `GST_IS_PAD_TEMPLATE (templ)' failed

_getAndLockVSLock: can not get lock vss_lock!

Can not create/open ipc semphone!

(gst-plugin-scanner:786): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_audio_pp.so': lib_peq_arm11y

(gst-plugin-scanner:786): GStreamer-CRITICAL **: gst_value_set_int_range: assertion `start < end' failed

(gst-plugin-scanner:786): GStreamer-CRITICAL **: gst_value_set_int_range: assertion `start < end' failed

(gst-plugin-scanner:786): GStreamer-CRITICAL **: gst_value_set_int_range: assertion `start < end' failed

(gst-plugin-scanner:786): GStreamer-CRITICAL **: gst_value_set_int_range: assertion `start < end' failed

(gst-plugin-scanner:786): GStreamer-CRITICAL **: gst_value_set_int_range: assertion `start < end' failed

(gst-plugin-scanner:786): GStreamer-CRITICAL **: gst_value_set_int_range: assertion `start < end' failed

(gst-launch-0.10:785): GStreamer-CRITICAL **: gst_element_class_add_pad_template: assertion `GST_IS_PAD_TEMPLATE (templ)' failed

(gst-launch-0.10:785): GStreamer-CRITICAL **: gst_pad_new_from_template: assertion `GST_IS_PAD_TEMPLATE (templ)' failed

(gst-launch-0.10:785): GStreamer-CRITICAL **: gst_pad_set_activate_function: assertion `GST_IS_PAD (pad)' failed

(gst-launch-0.10:785): GStreamer-CRITICAL **: gst_pad_set_activatepull_function: assertion `GST_IS_PAD (pad)' failed

(gst-launch-0.10:785): GStreamer-CRITICAL **: gst_pad_set_activatepush_function: assertion `GST_IS_PAD (pad)' failed

(gst-launch-0.10:785): GStreamer-CRITICAL **: gst_pad_set_chain_function: assertion `GST_IS_PAD (pad)' failed

(gst-launch-0.10:785): GStreamer-CRITICAL **: gst_pad_set_event_function: assertion `GST_IS_PAD (pad)' failed

(gst-launch-0.10:785): GStreamer-CRITICAL **: gst_element_add_pad: assertion `GST_IS_PAD (pad)' failed

(gst-launch-0.10:785): GStreamer-CRITICAL **: gst_pad_set_setcaps_function: assertion `GST_IS_PAD (pad)' failed

I think gstreamer-WARNING are due to absence of the libraries which is shown in the error message itself.

Can you please help to fix the gstreamer-CRITICAL issues.

Labels (2)
Tags (1)
0 Kudos
Reply
2 Replies

675 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ravi

please install codecs from

Codecs and other Algorithms (1)

"Linux Multimedia Codecs Documentation and Sources 11.09 for i.MX53 for the Quick

Start boards.Updated with the Linux 11.09 patch release and the 2.0.5 Open Max files. (REV 2011.09.03)

i.MX53 Quick Start Board|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

675 Views
kravik
Contributor IV

I have built multimedia image using yocto and is working fine. Thanks.

0 Kudos
Reply