when I use command " gst-launch-1.0 -v v4l2src device=/dev/video2 ! "video/x-raw, format=YUY2, width=1920, height=1080, framerate=60/1, pixel-aspect-ratio=1/1, interlace-mode=progressive, colorimetry=bt709" ! queue ! waylandsink" to display preview camera, the display window always presents fullscreen (I use a 4K resolution monitor), i.e., the video window is 1920*1080 and other part of the windows is black. How can I set the display window of gst-launch to the actual resolution (1920*1080)?
could you give me a picture to show this? and tell me what bsp version you use
I did more tests: (I used 5.15.71 BSP version, my own 1080p CMOS sensor, and a 1080p monitor)
could you please tell me why there are differences of window size with dewarp bypass or not bypass?
As I known, if you use ISP, you need enable dewarp in the same time, why do you need disable this?
I was just testing imaging effect directly from ISP. At now, I have not calibrated my dewarp parameters. Also, my lens don't have large distortion. Therefore, I temporily bypass it.
in dts file, if you disable dwe, the isp should be issue, if you want to bypass dewarp, you can set the "bypass" as true in dewarp config file