Setting pipeline to PAUSED ...
[INFO] Product Info: i.MX6Q/D/S
====== VPUENC: 4.0.8 build on Dec 15 2015 12:18:29. ======
wrapper: 1.0.62 (VPUWRAPPER_ARM_LINUX Build on Dec 15 2015 11:24:32)
vpulib: 5.4.32
firmware: 3.1.1.46070
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Internal data flow error.
Additional debug info:
/home/tangb/yocto/imx-3.14.52-1.1.0_ga/build-x11/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0/1.4.5-r0/gstreamer-1.4.5/libs/gst/base/gstbasesrc.c(2933): gst_base_src_loop (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
streaming task paused, reason not-negotiated (-4)
Execution ended after 0:00:00.122682333
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Freeing pipeline ...
i use usb camera.
the following command is OK ,it run well .
$GSTL v4l2src device=/dev/video0 ! 'video/x-raw,width=640,height=480' ! imxv4l2sink
but follow cmmmand is error and you knwned.
gst-launch-1.0 v4l2src device=/dev/video0 ! vpuenc_h264 ! rtph264pay ! udpsink host=192.168.1.111