Hay Guys,
i currently try to build a yocto and got the following Problem:
- If i Compile the Image with xwayland and without Chrome all is fine
- If i try to make a Image with Chrome-Ozone-Wayland it crash after 70% while "do_compile"
- If i try to Build the Chromium standalone "bitbake chrome-ozone-wayland" ti allso stucks at 70%
Can anyone help to fix this Issue?
解決済! 解決策の投稿を見る。
Hay,
so the issue was "to low memory". My Build PC have 8 Gbyte, i got the error with this. And with 16GByte all is fine
Hay,
so the issue was "to low memory". My Build PC have 8 Gbyte, i got the error with this. And with 16GByte all is fine
Hello Thomas Stockklauser,
Does this problem still continue?
Would you please provide more information on which BSP you are using?
Regards,