Hi,
I am using imx6q sabresd board.I am trying to build the gstreamer plugins.For the gstreamer to work,the package gst-fsl-plugins is required.But as i enable this package,I mam getting the following logs-
Processing: firmware-imx
=========================
Processing: imx-lib
=====================
Processing: imx-test
======================
Processing: kobs-ng
=====================
Processing: libfslcodec
=========================
Build path taken because: no prebuilt rpm,
Testing network connectivity
OK GPP:
Try libfslcodec-3.0.7.tar.gz.md5 from the GPP
http://bitshrine.org/gpp/libfslcodec-3.0.7.tar.gz.md5:
09:25:46 ERROR 404: Not Found.
Try libfslcodec-3.0.7.tar.gz from the GPP
http://bitshrine.org/gpp/libfslcodec-3.0.7.tar.gz:
09:25:51 ERROR 404: Not Found.
Can't get: libfslcodec-3.0.7.tar.gz at ./ltib line 802.
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Wed Jun 5 09:22:28 2013
Ended: Wed Jun 5 09:25:51 2013
Elapsed: 203 seconds
These packages failed to build:
libfslcodec
Build Failed
Can anybody please help me with this issue?
解決済! 解決策の投稿を見る。
please go to edit the ltib/dist/lfs-5.1/gst-plugins-good/gst-plugins-good.spec
use # to comment out the followings cairo things like this :
#export CAIRO_CFLAGS=-I/home/ashish/Desktop/dev_imx6/ltib/rootfs/usr/include/cairo
#export CAIRO_LIBS=-L/home/ashish/Desktop/dev_imx6/ltib/rootfs/usr/lib/cairo
#export LIBS=-lcairo
Hi Leo,
I was able to compile gst-fsl-plugins properly and can also use this command,
gst-launch v4l2src device=/dev/video1 ! ffmpegcolorspace ! mfw_v4lsink.
I just had to add ffmpegcolorspace to what you gave me before for web camera to start and capture the video.
Can you please tell me how can I save the captured video?
Check the filesink gst element. In case you need to store the encoded video, you also need to add a encoder element into the pipeline.
Leo
Please download the Multimedia Codec package from here:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW
Thnx jimmychan..It worked!
I am having problem building ltib with gst-plugins-good.
Processing: gst-plugins-good
==============================
Build path taken because: directory build, build key set, no prebuilt rpm,
rpmbuild --dbpath /home/ashish/Desktop/dev_imx6/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /home/ashish/Desktop/dev_imx6/ltib/rpm' --define '_prefix /usr' --define '_tmppath /home/ashish/Desktop/dev_imx6/ltib/tmp' --define '_rpmdir /home/ashish/Desktop/dev_imx6/ltib/rpm/RPMS' --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bc --short-circuit /home/ashish/Desktop/dev_imx6/ltib/dist/lfs-5.1/gst-plugins-good/gst-plugins-good.spec
Building target platforms: arm
Building for target arm
Executing(%build): /bin/sh -e /home/ashish/Desktop/dev_imx6/ltib/tmp/rpm-tmp.26615
+ umask 022
+ cd /home/ashish/Desktop/dev_imx6/ltib/rpm/BUILD
+ cd gst-plugins-good-0.10.30
+ export CAIRO_CFLAGS=-I/home/ashish/Desktop/dev_imx6/ltib/rootfs/usr/include/cairo
+ export CAIRO_LIBS=-L/home/ashish/Desktop/dev_imx6/ltib/rootfs/usr/lib/cairo
+ export LIBS=-lcairo
+ ./configure --prefix=/usr --host=arm-linux --build=i686-pc-linux-gnu --without-check --disable-speex --disable-shout2test --disable-shout2 --disable-dv1394 --disable-libpng --disable-libdv --disable-libcaca --disable-ladspa --disable-jpeg --disable-flac --disable-esd --disable-esdtest --disable-cairo --disable-aalib --disable-aalibtest --disable-x --disable-xvideo --disable-hal NM=nm
configure: WARNING: unrecognized options: --without-check, --disable-ladspa
checking for a BSD-compatible install... /usr/bin/install -c
checking whether build environment is sane... yes
checking for arm-linux-strip... arm-linux-strip
checking for a thread-safe mkdir -p... /bin/mkdir -p
checking for gawk... gawk
checking whether make sets $(MAKE)... yes
checking nano version... 0 (release)
checking whether to enable maintainer-specific portions of Makefiles... no
checking build system type... i686-pc-linux-gnu
checking host system type... arm-unknown-linux-gnu
checking how to print strings... printf
checking for style of include used by make... GNU
checking for arm-linux-gcc... gcc
checking whether the C compiler works... no
configure: error: in `/home/ashish/Desktop/dev_imx6/ltib/rpm/BUILD/gst-plugins-good-0.10.30':
configure: error: C compiler cannot create executables
See `config.log' for more details
error: Bad exit status from /home/ashish/Desktop/dev_imx6/ltib/tmp/rpm-tmp.26615 (%build)
RPM build errors:
Bad exit status from /home/ashish/Desktop/dev_imx6/ltib/tmp/rpm-tmp.26615 (%build)
Build time for gst-plugins-good: 1 seconds
Failed building gst-plugins-good
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Wed Jun 5 12:57:04 2013
Ended: Wed Jun 5 12:57:06 2013
Elapsed: 2 seconds
These packages failed to build:
gst-plugins-good
Build Failed
Exiting on error or interrupt
please go to edit the ltib/dist/lfs-5.1/gst-plugins-good/gst-plugins-good.spec
use # to comment out the followings cairo things like this :
#export CAIRO_CFLAGS=-I/home/ashish/Desktop/dev_imx6/ltib/rootfs/usr/include/cairo
#export CAIRO_LIBS=-L/home/ashish/Desktop/dev_imx6/ltib/rootfs/usr/lib/cairo
#export LIBS=-lcairo
Thnx Jimmy!
I am able to build my ltib with gstreamer-plugins-good , gst-fsl-plugins and gst-fsl-plugins.I am able to play the default video which is under unit_tests but i am not able to play any other video other than the default one.
gplay Cutie.mpeg
playbin2 is employed!
fsl_player_init(): Successfully initialize!
fsl_player_set_media_location(): filename=Cutie.mpeg
[Stopped ][Vol=01][00:00:00/00:00:00][fps:0]Aiur: 3.0.7
Core: BLN_MAD-MMLAYER_MPG2PARSER_04.04.11 build on Feb 21 2013 14:11:55
mime: video/mpeg, mpegversion=(int)[1,2]; video/mpegts, systemstream=true; video/x-cdxa
file: /usr/lib/imx-mm/parser/lib_mpg2_parser_arm11_elinux.so.3.1
Content Info:
URI:
file:///home/user/Cutie.mpeg
Idx File:
/root/.aiur/.home.user.Cutie.mpeg.aidx
Seekable : Yes
Size(byte): 4866460
Mpeg2CreateParser:parser created successfully
Movie Info:
Seekable : Yes
Live : No
Duration : 0:01:03.900000000
ReadMode : File
programs : 1
Track : 2
Track 00 [video_000000] Enabled
ppid: 0, ppid 0
Duration: 0:01:03.880000000
Language: und
Mime:
video/mpeg, systemstream=(boolean)false, parsed=(boolean)true, mpegversion=(int)
2, width=(int)320, height=(int)240, framerate=(fraction)25/1, codec_data=(buffer
)000001b31400f0130138a0a51011111212121313131314141414141515151515151616161616161
6171717171717171718181818181818191a191a1a191b1b1b1a1b1c1c1c1c1e1e1e1f1f21000001b
800080040
Track 01 [audio_000001] Enabled
ppid: 0, ppid 1
Duration: 0:01:03.900000000
Language: und
Mime:
audio/mpeg, mpegversion=(int)1, framed=(boolean)true, channels=(int)1, rate=(int
)32000, bitrate=(int)96
Aiur: 3.0.7
Core: BLN_MAD-MMLAYER_MPG2PARSER_04.04.11 build on Feb 21 2013 14:11:55
mime: video/mpeg, mpegversion=(int)[1,2]; video/mpegts, systemstream=true; video/x-cdxa
file: /usr/lib/imx-mm/parser/lib_mpg2_parser_arm11_elinux.so.3.1
Content Info:
URI:
file:///home/user/Cutie.mpeg
Idx File:
/root/.aiur/.home.user.Cutie.mpeg.aidx
Seekable : No
Size(byte): -1
FOUND GST_MESSAGE_TAG!
codec: MPEG2
language code: und
bitrate: 500000
FOUND GST_MESSAGE_TAG!
container format: MPEG
FOUND GST_MESSAGE_TAG!
codec: MP3
language code: und
bitrate: 96
state change failed from 2 to 4
try to play failed
Debug: aiurdemux.c(4262): aiurdemux_push_task (): /GstPlayBin2:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20/GstAiurDemux:aiurdemux1:
streaming stopped, reason error
Error: GStreamer encountered a general stream error.
[Stopped ][Vol=01][00:00:00/00:00:00][fps:0]
FSL_PLAYER_01.00_LINUX build on Jun 5 2013 12:55:46
[h]display the operation Help
[p]Play
[s]Stop
[e]Seek
[a]Pause when playing, play when paused
[v]Volume
fsl_player_stop()
[m]Switch to mute or not
[>]Play next file
[<]Play previous file
[r]Switch to repeated mode or not
[f]Set full screen or not
[z]resize the width and height
[t]Rotate
[c]Setting play rate
[i]Display the metadata
[x]eXit
FSL_PLAYER_UI_MSG_INTERNAL_ERROR: internal error message received.
fsl_player_stop()
player_exit(): No more multimedia files, exit.
[Stopped ][Vol=01][00:00:00/00:00:00][fps:0]g_main_loop_thread_fun() quit!
fsl_player_deinit
Can u please help with playing videos??
hi,the FSL_PLAYER_UI_MSG_INTERNAL_ERROR: internal error message received. ,are you ok ? i have the same qustion
Please check the Release Note of the Multimedia codes. Due to license limitation, not all the video formats supported. If you have any new question/problem, it is better to create another new post. Thanks. :smileyhappy:
Hello jimmychan,
I am using iMX6 Sololite board and I have been trying to build gstreamer plugin. I am getting similar error as given above when I am trying to enable gst-fsl-plugin. I went to gst-plugins-good spec file but there was no cairo in my gst-plugins-good spec file. In my spec file it has following things:
%Build
./configure --prefix=%{_prefix} --host=$CFGHOST \
--build=%{_build} --without-check \
--disable-speex \
--disable-shout2test --disable-shout2 \
--disable-dv1394 --disable-libpng \
--disable-libdv --disable-libcaca \
--disable-ladspa --disable-jpeg \
--disable-flac \
--disable-esd --disable-esdtest \
--disable-cairo --disable-aalib \
--disable-aalibtest --disable-x \
--disable-xvideo --disable-hal NM=nm
Here is my error. Please I need your help. It is very urgent.
Processing: libfslcodec
=========================
Processing: libfslparser
==========================
Processing: gst-fsl-plugins
=============================
Build path taken because: directory build, no prebuilt rpm,
scbuild/scdeploy already unpacked package
Processing: gst-fsl-plugins
=============================
Build path taken because: directory build, build key set, no prebuilt rpm,
rpmbuild --dbpath /home/pshah9/Documents/imx6install/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /home/pshah9/Documents/imx6install/ltib/rpm' --define '_prefix /usr' --define '_tmppath /home/pshah9/Documents/imx6install/ltib/tmp' --define '_rpmdir /home/pshah9/Documents/imx6install/ltib/rpm/RPMS' --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bc --short-circuit /home/pshah9/Documents/imx6install/ltib/dist/lfs-5.1/fsl-mm/gst-fsl-plugins.spec
Building target platforms: arm
Building for target arm
Executing(%build): /bin/sh -e /home/pshah9/Documents/imx6install/ltib/tmp/rpm-tmp.82439
+ umask 022
+ cd /home/pshah9/Documents/imx6install/ltib/rpm/BUILD
+ cd gst-fsl-plugins-3.0.3
+ which pkg-config
+ export PKG_CONFIG=/opt/freescale/ltib/usr/bin/pkg-config --static
+ echo imx6s
+ sed s,imx\([0-9]*\).*,MX\1,g
+ PLATFORMSHORTNAME=MX6
+ [ xMX6 = xMX27 ]
+ export FBHEADER_PATH=/home/pshah9/Documents/imx6install/ltib/rootfs/usr/src/linux/include/
+ echo imx6s
+ sed s,imx\([0-9]*\).*,MX\1,g
+ ./autogen.sh PLATFORM=MX6
+ aclocal
+ libtoolize --force
libtoolize: putting auxiliary files in `.'.
libtoolize: linking file `./ltmain.sh'
libtoolize: putting macros in AC_CONFIG_MACRO_DIR, `m4'.
libtoolize: linking file `m4/libtool.m4'
libtoolize: linking file `m4/ltoptions.m4'
libtoolize: linking file `m4/ltsugar.m4'
libtoolize: linking file `m4/ltversion.m4'
libtoolize: linking file `m4/lt~obsolete.m4'
+ automake -a
Makefile.am:947: `%'-style pattern rules are a GNU make extension
+ autoconf
+ conf_flags=--enable-maintainer-mode
+ test x = x
+ echo Running ./configure --enable-maintainer-mode PLATFORM=MX6 ...
Running ./configure --enable-maintainer-mode PLATFORM=MX6 ...
+ ./configure --enable-maintainer-mode PLATFORM=MX6
checking for a BSD-compatible install... /usr/bin/install -c
checking whether build environment is sane... yes
checking for a thread-safe mkdir -p... /bin/mkdir -p
checking for gawk... no
checking for mawk... mawk
checking whether make sets $(MAKE)... yes
checking whether to enable maintainer-specific portions of Makefiles... yes
checking for gcc... gcc
checking whether the C compiler works... yes
checking for C compiler default output file name... a.out
checking for suffix of executables...
checking whether we are cross compiling... no
checking for suffix of object files... o
checking whether we are using the GNU C compiler... yes
checking whether gcc accepts -g... yes
checking for gcc option to accept ISO C89... none needed
checking for style of include used by make... GNU
checking dependency style of gcc... gcc3
checking whether gcc and cc understand -c and -o together... yes
checking build system type... x86_64-unknown-linux-gnu
checking host system type... x86_64-unknown-linux-gnu
checking how to print strings... printf
checking for a sed that does not truncate output... /bin/sed
checking for grep that handles long lines and -e... /bin/grep
checking for egrep... /bin/grep -E
checking for fgrep... /bin/grep -F
checking for ld used by gcc... ld
checking if the linker (ld) is GNU ld... yes
checking for BSD- or MS-compatible name lister (nm)... /usr/bin/nm -B
checking the name lister (/usr/bin/nm -B) interface... BSD nm
checking whether ln -s works... yes
checking the maximum length of command line arguments... 1572864
checking whether the shell understands some XSI constructs... yes
checking whether the shell understands "+="... yes
checking how to convert x86_64-unknown-linux-gnu file names to x86_64-unknown-linux-gnu format... func_convert_file_noop
checking how to convert x86_64-unknown-linux-gnu file names to toolchain format... func_convert_file_noop
checking for ld option to reload object files... -r
checking for objdump... objdump
checking how to recognize dependent libraries... pass_all
checking for dlltool... no
checking how to associate runtime and link libraries... printf %s\n
checking for archiver @FILE support... @
checking for strip... strip
checking for ranlib... ranlib
checking command to parse /usr/bin/nm -B output from gcc object... ok
checking for sysroot... no
checking for mt... mt
checking if mt is a manifest tool... no
checking how to run the C preprocessor... gcc -E
checking for ANSI C header files... yes
checking for sys/types.h... yes
checking for sys/stat.h... yes
checking for stdlib.h... yes
checking for string.h... yes
checking for memory.h... yes
checking for strings.h... yes
checking for inttypes.h... yes
checking for stdint.h... yes
checking for unistd.h... yes
checking for dlfcn.h... yes
checking for objdir... .libs
checking if gcc supports -fno-rtti -fno-exceptions... no
checking for gcc option to produce PIC... -fPIC -DPIC
checking if gcc PIC flag -fPIC -DPIC works... yes
checking if gcc static flag -static works... yes
checking if gcc supports -c -o file.o... yes
checking if gcc supports -c -o file.o... (cached) yes
checking whether the gcc linker (ld -m elf_x86_64) supports shared libraries... yes
checking whether -lc should be explicitly linked in... no
checking dynamic linker characteristics... GNU/Linux ld.so
checking how to hardcode library paths into programs... immediate
checking whether stripping libraries is possible... yes
checking if libtool supports shared libraries... yes
checking whether to build shared libraries... yes
checking whether to build static libraries... yes
checking for pkg-config... yes
configure: build for MX6
checking pkg-config is at least version 0.9.0... yes
checking for GST... no
configure: error: you need gstreamer development packages installed !
+ exit 1
error: Bad exit status from /home/pshah9/Documents/imx6install/ltib/tmp/rpm-tmp.82439 (%build)
RPM build errors:
Bad exit status from /home/pshah9/Documents/imx6install/ltib/tmp/rpm-tmp.82439 (%build)
Build time for gst-fsl-plugins: 14 seconds
Failed building gst-fsl-plugins
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Tue Jun 11 15:24:10 2013
Ended: Tue Jun 11 15:41:34 2013
Elapsed: 1044 seconds
These packages failed to build:
gst-fsl-plugins
Build Failed
Exiting on error or interrupt
I believe you are building this packages independently (with ltib -p , this way if pkg dependencies are not present on target, then you get a configuration error, the error you are seeing). It is best to select the good package from the ltib menu, then save configuartion and run ltib again (no arguments). This way you got all package dependencies included.
Leo
After selecting gst-fsl-plugin, I am just running ./ltib (without any arguments).
I have installed all of these gstreamer development packages.
sudo apt-get install libdbus-1-dev libdbus-glib-1-dev libgstreamer0.10-dev libreadline-dev libgstreamer-plugins-base0.10-dev