Dear guys,
I have one OS yocto 2.4 rock (kernel 4.9.88) which runs in imx6q, the gpu and vpu work well.
So I try another OS yocto 3.1 Zeus(kernel 5.4.47)which runs in imx6q, the gpu and vpu don't work.
Log as below
[ 3.850835] galcore 130000.gpu: ignoring dependency for device, assuming no driver
[ 3.858990] mxc_vpu 2040000.vpu_fsl: ignoring dependency for device, assuming no driver
Could somebody help me?
已解决! 转到解答。
Hi igor,
I found the reason that is my custom board remove the pmic.
So I comment some dts item as below
/*
®_arm {
vin-supply = <&sw1a_reg>;
};
®_pu {
vin-supply = <&sw1c_reg>;
};
®_soc {
vin-supply = <&sw1c_reg>;
};
*/
Now the GPU & VPU can work well.
Hi zohanlin
one can try to test vpu,gpu on nxp sabresd reference board with Demo Image
i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualLite, i.MX 6SoloX Boards
Best regards
igor
Hi igor,
I found the reason that is my custom board remove the pmic.
So I comment some dts item as below
/*
®_arm {
vin-supply = <&sw1a_reg>;
};
®_pu {
vin-supply = <&sw1c_reg>;
};
®_soc {
vin-supply = <&sw1c_reg>;
};
*/
Now the GPU & VPU can work well.
I found a post about the issue.
Bio_TICFSL said : Sorry and yes the issue is on DTBs.
Is it really?
I tried to modify dts and set #power-domain-cells by <1>
--------------------------------------------------------------------------
pd_pu: power-domain@1 {
reg = <1>;
#power-domain-cells = <1>;
power-supply = <®_pu>;
clocks = <&clks IMX6QDL_CLK_GPU3D_CORE>,
<&clks IMX6QDL_CLK_GPU3D_SHADER>,
<&clks IMX6QDL_CLK_GPU2D_CORE>,
<&clks IMX6QDL_CLK_GPU2D_AXI>,
<&clks IMX6QDL_CLK_OPENVG_AXI>,
<&clks IMX6QDL_CLK_VPU_AXI>;
};
Now the log is
root@imx6qsabresd:~# dmesg | grep -i "gpu"
[ 3.628942] OF: /soc/gpu@00130000: #power-domain-cells = 1 found -1
[ 4.328302] galcore: probe of 130000.gpu failed with error -22
root@imx6qsabresd:~# dmesg | grep -i "gal"
[ 3.291714] egalax_ts 1-0004: Failed to switch to I2C interface
[ 3.298098] egalax_ts 2-0004: Failed to switch to I2C interface
[ 3.636502] Galcore version 6.4.3.p0.286725
[ 4.291168] [galcore]: Feature database is not found,chipModel=0x0, chipRevision=0x0, productID=0x0, ecoID=0x0, customerID=0x0
[ 4.328302] galcore: probe of 130000.gpu failed with error -22
root@imx6qsabresd:~# dmesg | grep -i "vpu"
[ 4.334554] OF: /soc/aips-bus@2000000/vpu_fsl@2040000: #power-domain-cells = 1 found -1
[ 4.343296] mxc_vpu 2040000.vpu_fsl: VPU initialized