gpmi-nfc gpmi-nfc.0: [read_page] DMA error on IMX28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gpmi-nfc gpmi-nfc.0: [read_page] DMA error on IMX28

1,178 Views
hongyuplim
Contributor I

Hello,

I have a problem on my board based on IMX28

Generally it works well, but sometimes I met kernel panic problem,

here is booting log.

Please give me a help and advice.

Thanks all.

=========================================================================================

HTLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLFLCHW_RTC_PERSISTENT1_RD = [0x00000800]

PowerPrep start initialize power...

Configured for 5v only power source.           Battery powered operation disabled.
LLLCMay 28 201416:16:17
FRAC 0x92925552
memory type is W9751G6JB DDR2
                             Wait for ddr ready 1power 0x00820710
Frac 0x92925552
start change cpu freq
hbus 0x00000003
cpu 0x00010001
LLLLLLLFLCLLJUncompressing Linux... done, booting the kernel.
Linux version 2.6.35.3-670-g914558e (hylim@hylim-virtual-machine) (gcc version 4.4.4 (4.4.4_09.06.2010) ) #1169 PREEMPT Wed Jul 23 21:07:08 KST 2014
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: Freescale MX28EVK board
Memory policy: ECC disabled, Data cache writeback
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 16256
Kernel command line: noinitrd console=ttyAM0,115200 consoleblank=0 ubi.mtd=2 root=ubi0:rootfs0 rootfstype=ubifs rw gpmi splash=silent
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory: 64MB = 64MB total
Memory: 56100k/56100k available, 9436k reserved, 0K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    DMA     : 0xfde00000 - 0xffe00000   (  32 MB)
    vmalloc : 0xc4800000 - 0xf0000000   ( 696 MB)
    lowmem  : 0xc0000000 - 0xc4000000   (  64 MB)
    modules : 0xbf000000 - 0xc0000000   (  16 MB)
      .init : 0xc0008000 - 0xc002b000   ( 140 kB)
      .text : 0xc002b000 - 0xc042a000   (4092 kB)
      .data : 0xc042a000 - 0xc0462c20   ( 228 kB)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
        RCU-based detection of stalled CPUs is disabled.
        Verbose stalled-CPUs detection is disabled.
NR_IRQS:288
Console: colour dummy device 80x30
console [ttyAM0] enabled
Calibrating delay loop... 226.09 BogoMIPS (lpj=1130496)
pid_max: default: 32768 minimum: 301
Security Framework initialized
SELinux:  Initializing.
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
regulator: core version 0.5
NET: Registered protocol family 16
regulator: vddd: 800 <--> 1575 mV at 1500 mV fast normal
regulator: vdddbo: 800 <--> 1575 mV fast normal
regulator: vdda: 1500 <--> 2275 mV at 1800 mV fast normal
vddio = 3380000, val=10
regulator: vddio: 2880 <--> 3680 mV at 3380 mV fast normal
regulator: overall_current: fast normal
regulator: vbus5v:
regulator: mxs-duart-1: fast normal
regulator: mxs-bl-1: fast normal
regulator: mxs-i2c-1: fast normal
regulator: mmc_ssp-1: fast normal
regulator: mmc_ssp-2: fast normal
regulator: charger-1: fast normal
regulator: power-test-1: fast normal
regulator: cpufreq-1: fast normal
i.MX IRAM pool: 124 KB@0xc4820000
Initializing GPMI pins
usb DR wakeup device is registered
IMX usb wakeup probe
audit: cannot initialize inotify handle
bio: create slab <bio-0> at 0
SCSI subsystem initialized
Freescale USB OTG Driver loaded, $Revision: 1.55 $
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Switching to clocksource mxs clock source
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (junk in compressed archive); looks like an initrd
Freeing initrd memory: 4096K
Bus freq driver module loaded
IMX usb wakeup probe
usb h1 wakeup device is registered
mxs_cpu_init: cpufreq init finished
audit: initializing netlink socket (disabled)
type=2000 audit(0.790:1): initialized
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
JFFS2 version 2.2. (NAND) 짤 2001-2006 Red Hat, Inc.
msgmni has been set to 117
alg: No test for stdrng (krng)
cryptodev: driver loaded.
Block layer SCSI generic (bsg) driver version 0.4 loaded (major 253)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Console: switching to colour frame buffer device 60x17
mxs-duart.0: ttyAM0 at MMIO 0x80074000 (irq = 47) is a DebugUART
mxs-auart.0: ttySP0 at MMIO 0x8006a000 (irq = 112) is a mxs-auart.0
Found APPUART 3.1.0
mxs-auart.1: ttySP1 at MMIO 0x8006c000 (irq = 113) is a mxs-auart.1
Found APPUART 3.1.0
mxs-auart.2: ttySP2 at MMIO 0x8006e000 (irq = 114) is a mxs-auart.2
Found APPUART 3.1.0
mxs-auart.3: ttySP3 at MMIO 0x80070000 (irq = 115) is a mxs-auart.3
Found APPUART 3.1.0
mxs-auart.4: ttySP4 at MMIO 0x80072000 (irq = 116) is a mxs-auart.4
Found APPUART 3.1.0
brd: module loaded
loop: module loaded
i.MX GPMI NFC
NFC: Version 1, 8-chip GPMI and BCH
Boot ROM: Version 1, Single-chip boot area, block mark swapping supported
Scanning for NAND Flash chips...
NAND device: Manufacturer ID: 0x01, Chip ID: 0xf1 (AMD NAND 128MiB 3,3V 8-bit)
-----------------------------
NAND Flash Device Information
-----------------------------
Manufacturer      : AMD (0x01)
Device Code       : 0xf1
Cell Technology   : SLC
Chip Size         : 128 MiB
Pages per Block   : 64
Page Geometry     : 2048+64
ECC Strength      : 4 bits
ECC Size          : 512 B
Data Setup Time   : 10 ns
Data Hold Time    : 5 ns
Address Setup Time: 10 ns
GPMI Sample Delay : 6 ns
tREA              : Unknown
tRLOH             : Unknown
tRHOH             : Unknown
Description       : S34ML01G1
-----------------
Physical Geometry
-----------------
Chip Count             : 1
Page Data Size in Bytes: 2048 (0x800)
Page OOB Size in Bytes : 64
Block Size in Bytes    : 131072 (0x20000)
Block Size in Pages    : 64 (0x40)
Chip Size in Bytes     : 134217728 (0x8000000)
Chip Size in Pages     : 65536 (0x10000)
Chip Size in Blocks    : 1024 (0x400)
Medium Size in Bytes   : 134217728 (0x8000000)
------------
NFC Geometry
------------
ECC Algorithm          : BCH
ECC Strength           : 8
Page Size in Bytes     : 2112
Metadata Size in Bytes : 10
ECC Chunk Size in Bytes: 512
ECC Chunk Count        : 4
Payload Size in Bytes  : 2048
Auxiliary Size in Bytes: 16
Auxiliary Status Offset: 12
Block Mark Byte Offset : 1999
Block Mark Bit Offset  : 0
-----------------
Boot ROM Geometry
-----------------
Boot Area Count            : 1
Boot Area Size in Bytes    : 10485760 (0xa00000)
Stride Size in Pages       : 64
Search Area Stride Exponent: 2
Scanning device for bad blocks
Boot area protection is enabled.
Creating 4 MTD partitions on "gpmi-nfc-main":
0x000000000000-0x000000a00000 : "gpmi-nfc-kernel"
0x000000a00000-0x000001400000 : "gpmi-nfc-kernel2"
0x000001400000-0x000007000000 : "gpmi-nfc-general-use"
0x000007000000-0x000008000000 : "gpmi-nfc-user"
UBI: attaching mtd2 to ubi0
UBI: physical eraseblock size:   131072 bytes (128 KiB)
UBI: logical eraseblock size:    126976 bytes
UBI: smallest flash I/O unit:    2048
UBI: VID header offset:          2048 (aligned 2048)
UBI: data offset:                4096
gpmi-nfc gpmi-nfc.0: [gpmi_nfc_dma_go] Chip: 0, DMA Channel: 4, Error -110
gpmi-nfc gpmi-nfc.0: [read_page] DMA error

======================================================================================

Tags (3)
0 Kudos
2 Replies

632 Views
igorpadykov
NXP Employee
NXP Employee

Hi honguyp

I agree, probably more newer kernel may help.

Please look for example below

Use NAND-Flash with Kernel 3.2 on mx28evk

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

632 Views
michelleweng
Contributor I

Hi, Hongyup:

We meet the same problem in imx287, linux2.6.35, gcc4.4.4. I mean most of the time the system works well, only sometimes reboot will fail and we can see the error informations in serial bus. After power cycle, it will recover. It seems like that in gpmi_nfc_dma_go(), it waits for the dma_done flag, which will be set in gpmi_nfc_dma_isr(). When something goes wrong, isr doesn't work and kernel will be stuck in DMA error.

We are not familiar with the gpmi driver and maybe there are some bugs inside. Anyway we have tried some ways including reboot the kernel when DMA error happens, but can't figure it out yet.

We also try to contact with freescale's FAE, no response either.

If you have any updates for this please also let us know. Thanks.

0 Kudos