google chrome on imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

google chrome on imx6

1,853 Views
sameerarvikar
Contributor III

Hi ,

I want to install google chrome on imx6 on linux ,

Which yocto version supports it .

I know chromium browser can be install ,but is it possible to install chrome

thanks & regards

0 Kudos
1 Reply

904 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

From NXP Yocto BSP side, just the Chromium recipe is available. Another option could be using a different Linux BSP for i.MX6 with Chrome support, like Ubuntu and try on it:

You could take a look at the following link:

https://community.nxp.com/docs/DOC-330147

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos