with below log,
../../../../gstreamer-1.6.3/libs/gst/base/gstbasesink.c(2846): gst_base_sink_is_too_late (): /GstPipeline:pipeline0/GstGLImageSinkBin:glimagesinkbin0/GstGLImageSink:sink:
There may be a timestamping problem, or this computer is too slow.
Not initialized
Can you please help us on,
1. why CPU is taking more?
2. Lib egl verison What we need to use.
3. Video struck issue.
Thanks,
Arunkumar R
Hi Arunkumar Rajagopal, let me check with the team.
Let me check again,
b36401 can you help to continue with the follow up?
Hi,
Still we are struggling to fix this issue. We need your support to proceed further.
Please understand.
Thanks,
Arunkumar R
It seems hardware acceleration was missing with such misversioning.
Please try the version that match.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Can you please remove "Assumed Answer" @Victor Linnik
As per the discussion with team here in Banglore. The latest egl version is 1.4.0
That version only we are using in our target.
Please find the attached build details below.
meta-fsl-arm:
fetch:yocto
brach : krogoth
last commit id:568edf983f52823398262a8266955a17fa9c60fa
commit msg: imx-kobs: Drop 5.4 recipe
openembedded-core:
fetch: github
branch: krogoth
last commit: a8f44dff13481feaa97e494a3aeafb5b63d40f3f
commit msg : binutils: fix AR issue when opkg is unpacking IPKs containing empty entries
last commit date: Date: Sun Jul 31 18:52:41 2016 +0000
gstreamer:
package for glimagesink: gstreamer1.0-plugins-bad_1.6.3.bb
SRC_URI = " \
http://gstreamer.freedesktop.org/src/gst-plugins-bad/gst-plugins-bad-${PV}.tar.xz \
EXTRA_OECONF += "--enable-gles2 "
Failure:
configure:34306: checking for WAYLAND_EGL
configure:34313: $PKG_CONFIG --exists --print-errors "wayland-client >= 1.0 wayland-cursor >= 1.0 wayland-egl >= 9.0"
Requested 'wayland-egl >= 9.0' but version of wayland-egl is 1.0.0
configure:34316: $? = 1
configure:34330: $PKG_CONFIG --exists --print-errors "wayland-client >= 1.0 wayland-cursor >= 1.0 wayland-egl >= 9.0"
Requested 'wayland-egl >= 9.0' but version of wayland-egl is 1.0.0
configure:34333: $? = 1
configure:34347: result: no
Requested 'wayland-egl >= 9.0' but version of wayland-egl is 1.0.0
configure:34553: WARNING: X or Wayland is required for OpenGL support
configure:34833: WARNING: Could not find any OpenGL platforms to use such as CGL, WGL or GLX
configure:34837: WARNING: Could not find any window systems to use such as Cocoa, Win32API or X11
configure:35049: checking for GLeglImageOES
configure:35049: arm-oe-linux-gnueabi-gcc -march=armv7-a -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a9 --sysroot=/home/abenjam1/u321/u321_5.0/build/tmp/sysroots/u321-imx6 -c -O2 -pipe
-g -feliminate-unused-debug-types -fdebug-prefix-map=/home/abenjam1/u321/u321_5.0/build/tmp/work/cortexa9hf-neon-mx6qdl-oe-linux-gnueabi/gstreamer1.0-plugins-bad/1.6.3-r0=/usr/src/debu
g/gstreamer1.0-plugins-bad/1.6.3-r0 -fdebug-prefix-map=/home/abenjam1/u321/u321_5.0/build/tmp/sysroots/x86_64-linux= -fdebug-prefix-map=/home/abenjam1/u321/u321_5.0/build/tmp/sysroots/u
321-imx6= -DLINUX -DEGL_API_FB -DWL_EGL_PLATFORM conftest.c >&5
conftest.c: In function 'main':
conftest.c:69:13: error: 'GLeglImageOES' undeclared (first use in this function)
build dependencies:
"gstreamer1.0-plugins-bad" [label="gstreamer1.0-plugins-bad :1.6.3-r0\n/home/abenjam1/u321/u321_5.0/Eagle-Distribution/oe-core/meta/recipes-multimedia/gstreamer/gstreamer1.0-plugins-bad_1.6.3.bb"]
"gstreamer1.0-plugins-bad" -> "pkgconfig-native" [style=solid]
"gstreamer1.0-plugins-bad" -> "autoconf-native" [style=solid]
"gstreamer1.0-plugins-bad" -> "automake-native" [style=solid]
"gstreamer1.0-plugins-bad" -> "libtool-native" [style=solid]
"gstreamer1.0-plugins-bad" -> "libtool-cross" [style=solid]
"gstreamer1.0-plugins-bad" -> "gnu-config-native" [style=solid]
"gstreamer1.0-plugins-bad" -> "virtual/gettext" [style=solid]
"gstreamer1.0-plugins-bad" -> "gettext-native" [style=solid]
"gstreamer1.0-plugins-bad" -> "virtual/arm-oe-linux-gnueabi-gcc" [style=solid]
"gstreamer1.0-plugins-bad" -> "virtual/arm-oe-linux-gnueabi-compilerlibs" [style=solid]
"gstreamer1.0-plugins-bad" -> "virtual/libc" [style=solid]
"gstreamer1.0-plugins-bad" -> "gstreamer1.0" [style=solid]
"gstreamer1.0-plugins-bad" -> "glib-2.0-native" [style=solid]
"gstreamer1.0-plugins-bad" -> "gstreamer1.0-plugins-base" [style=solid]
"gstreamer1.0-plugins-bad" -> "libpng" [style=solid]
"gstreamer1.0-plugins-bad" -> "jpeg" [style=solid]
"gstreamer1.0-plugins-bad" -> "gobject-introspection" [style=solid]
"gstreamer1.0-plugins-bad" -> "gobject-introspection-native" [style=solid]
"gstreamer1.0-plugins-bad" -> "qemu-native" [style=solid]
"gstreamer1.0-plugins-bad" -> "bluez5" [style=solid]
"gstreamer1.0-plugins-bad" -> "bzip2" [style=solid]
"gstreamer1.0-plugins-bad" -> "curl" [style=solid]
"gstreamer1.0-plugins-bad" -> "libxml2" [style=solid]
"gstreamer1.0-plugins-bad" -> "openssl" [style=solid]
"gstreamer1.0-plugins-bad" -> "virtual/libgles2" [style=solid]
"gstreamer1.0-plugins-bad" -> "nettle" [style=solid]
"gstreamer1.0-plugins-bad" -> "neon" [style=solid]
"gstreamer1.0-plugins-bad" -> "orc" [style=solid]
"gstreamer1.0-plugins-bad" -> "orc-native" [style=solid]
"gstreamer1.0-plugins-bad" -> "librsvg" [style=solid]
"gstreamer1.0-plugins-bad" -> "sbc" [style=solid]
"gstreamer1.0-plugins-bad" -> "libsndfile1" [style=solid]
"gstreamer1.0-plugins-bad" -> "libusb1" [style=solid]
"gstreamer1.0-plugins-bad" -> "libgudev" [style=solid]
"gstreamer1.0-plugins-bad" -> "wayland" [style=solid]
"gstreamer1.0-plugins-bad" -> "virtual/egl" [style=solid]
"gstreamer1.0-plugins-bad" -> "libwebp" [style=solid]
Can you post what your pipeline is?
Please find the pipeline
$ gst-launch-1.0 filesrc location=./Video.mp4 typefind=true ! aiurdemux ! queue max-size-time=0 ! vpudec ! glimagesink
Thanks,
Arunkumar R
Thanks for your input @Victor Linnik
The libegl is coming from meta-fsl-arm which is freescale yocto layer.
The bb file provides the lib:
imx-gpu-viv_5.0.11.p8.4-hfp.bb
Where can we get the corresponding version of lib egl delivery?