hi,
I update the latest linux BSP release fsl-yocto-L4.9.11_1.0.0, and build successfully with bitbake core-image-base command, then flash the corresponding files to SD card. the new image can boot normally but after finish boot i can't input anything via serial console (e.g Ctrl+C). the boot log is in the attachment, Is there any mistake? i need help thank you!
解決済! 解決策の投稿を見る。
hi Rita,
I test the demo images and it can run OK, and i located the issue is using the wrong DTB file (zImage-imx6q-sabresd.dtb), what differences zImage-imx6q-sabresd.dtb with zImage-imx6qp-sabresd.dtb?
Hi,
Have you tried the demo images, does it work?
Best Regards
Rita
hi Rita,
I test the demo images and it can run OK, and i located the issue is using the wrong DTB file (zImage-imx6q-sabresd.dtb), what differences zImage-imx6q-sabresd.dtb with zImage-imx6qp-sabresd.dtb?
Hi jiangdong li,
The imx6qp-sabresd is another board.i.MX 6QuadPlus SABRE Development Board|NXP
Have a nice day
Rita