fsl-yocto-L4.9.11_1.0.0 console issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

fsl-yocto-L4.9.11_1.0.0 console issue

Jump to solution
1,530 Views
jiangdongli
Contributor II

hi,

   I update the latest linux BSP release fsl-yocto-L4.9.11_1.0.0, and build successfully with bitbake core-image-base command, then flash the corresponding files to SD card. the new image can boot normally but after finish boot i can't input anything via serial console (e.g Ctrl+C). the boot log is in the attachment, Is there any mistake? i need help thank you!

Labels (3)
0 Kudos
Reply
1 Solution
1,345 Views
jiangdongli
Contributor II

hi Rita,

   I test the demo images and it can run OK, and i located the issue is using the wrong DTB file (zImage-imx6q-sabresd.dtb), what differences zImage-imx6q-sabresd.dtb with zImage-imx6qp-sabresd.dtb?

View solution in original post

0 Kudos
Reply
3 Replies
1,345 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Have you tried the demo images, does it work?

Best Regards

Rita

0 Kudos
Reply
1,346 Views
jiangdongli
Contributor II

hi Rita,

   I test the demo images and it can run OK, and i located the issue is using the wrong DTB file (zImage-imx6q-sabresd.dtb), what differences zImage-imx6q-sabresd.dtb with zImage-imx6qp-sabresd.dtb?

0 Kudos
Reply
1,345 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi jiangdong li,

The imx6qp-sabresd is another board.i.MX 6QuadPlus SABRE Development Board|NXP 

Have a nice day

Rita

0 Kudos
Reply