fsl-image-validation-imx build failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

fsl-image-validation-imx build failed

5,614 次查看
alexeymodyanov
Contributor II

I use latest 4.14.98_2.0.0_ga version and try to build an image for imx6qp Sabre board

I use bitbake fsl-image-validation-imx command

Host system  Ubuntu 16.04

Here is part of log:

git -c core.fsyncobjectfiles=0 checkout -B imx_18.11 64441b79b83e0790008486779054e9da891537f3 failed with exit code 128, output:
git-lfs smudge -- 'data/images/1280x720.ppm': 1: git-lfs smudge -- 'data/images/1280x720.ppm': git-lfs: not found
error: external filter git-lfs smudge -- %f failed -1
error: external filter git-lfs smudge -- %f failed
fatal: data/images/1280x720.ppm: smudge filter lfs failed

ERROR: arm-compute-library-18.11+gitAUTOINC+64441b79b8-r0 do_unpack: Function failed: base_do_unpack

if I try to execute commands just in command line all works fine.

标签 (3)
8 回复数

4,369 次查看
jay_park
Contributor II

I got a same issue and solve it by adding a symbolic link of git-lfs in build/tmp/hosttools directory.

imx-yocto-bsp/build/tmp/hosttools$ ln -sf /usr/bin/git-lfs git-lfs

Hope it helps you. 

4,616 次查看
luciomonteros
Contributor I

The same happens to me in my imx8mq. Does anyone solve this error?

0 项奖励
回复

4,970 次查看
khang_letruong1
Contributor I

Hello All,

I've got same error by doing following commands as in the i.MX_Yocto_Project_User's_Guide.pdf :

$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.0.0_ga.xml
$ repo sync

$ DISTRO=fsl-imx-wayland MACHINE=imx8mmevk source fsl-setup-release.sh -b build-wayland
$ bitbake fsl-image-validation-imx

My laptop runs Ubuntu-16.04. What should I do?

Thanks in advance,

0 项奖励
回复

4,970 次查看
gn02380756
Contributor II

Hi Radhika Somaiya:

I faced the same problem when building imx6qsabresd, following is my error log.

build_error.PNG

I'm sure I had installed git-lfs, but the error still occurred. Can you please solve this problem? Thanks!

4,882 次查看
rohit_k
Contributor I

Hello,

I am also getting same error  while compilation..

Please see logs.

ERROR: arm-compute-library-18.11+gitAUTOINC+64441b79b8-r0 do_unpack: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-3BLvOBVse5"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/sources/poky/scripts:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot/usr/bin/crossscripts:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot-native/usr/sbin:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot-native/usr/bin:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot-native/sbin:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot-native/bin:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/sources/poky/bitbake/bin:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/hosttools"; export HOME="/home/rohit"; git -c core.fsyncobjectfiles=0 checkout -B imx_18.11 64441b79b83e0790008486779054e9da891537f3 failed with exit code 128, output:
git-lfs smudge -- 'data/images/1280x720.ppm': 1: git-lfs smudge -- 'data/images/1280x720.ppm': git-lfs: not found
error: external filter git-lfs smudge -- %f failed -1
error: external filter git-lfs smudge -- %f failed
fatal: data/images/1280x720.ppm: smudge filter lfs failed

ERROR: arm-compute-library-18.11+gitAUTOINC+64441b79b8-r0 do_unpack: Function failed: base_do_unpack
ERROR: Logfile of failure stored in: /home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/temp/log.do_unpack.4789
ERROR: Task (/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-support/arm-compute-library/arm-compute-library_git-imx.bb:do_unpack) failed with exit code '1'

 

Can you please tell me how you resolved ?  

Thank you!

Regards, 

Rohit

0 项奖励
回复

4,970 次查看
q325mg
Contributor II

I have the same issue but with IMX8 QXP MEK

Were you able to fix it alexeymodyanov

Thanks

Edit:

The way it worked for was: the first time I was using Ubuntu 16, and tried to create the image on a restricted network, so I had to manually disable SSL from git and https from python, and I got the error, then instead I created a clean new Ubuntu 18 installation and did the build on a unrestricted network and it worked

0 项奖励
回复

4,595 次查看
luciomonteros
Contributor I

How did you disable SSL from git and https from python ?

And then you copied all the files created in tmp in ubuntu 16 to ubuntu 18 ?

标记 (1)
0 项奖励
回复

4,970 次查看
radhikasomaiya
Senior Contributor II


Hi  Alexey Modyanov,

We are able to build image successfully for imx6qpsabresd by following the steps of attached Yocto User's guide version L4.14.98_2.0.0. Can you please try to fresh build?

For git-lfs: not found error, you can try to install git-lfs.

Refer this link for git-lfs installation.

Regards,

Radhika Somaiya.