Hi,All:
freescale imx6 sata code can be modified to use msata interface?
Because the sata code was written dead. (for linux 3.10.53 BSP)
I want to be able to modify MSATA_DEVSLP, MSATA_PWR_EN signal to someone pin.
Able to do it?
please help me,thanks.
(中譯: freescale imx6 sata code 能修改成msata 介面來用嗎?
因為sata code被寫死了。(針對linux3.10.53 BSP的code)
我想要能夠修改MSATA_DEVSLP, MSATA_PWR_EN信號到某一支pin上。
能夠做到嗎?
)
解決済! 解決策の投稿を見る。
Mr Chen,
It is called fixed regulator. "compatible = "regulator-fixed";"
You should have device tree knowledge to read the dts file.
It's got nothing to do with sata. it is power supply.
For the MSATA_PWR_EN
Please follow binding guide Documentation\devicetree\bindings\regulator fixed-regulator.txt, add your gpio regulator.
And gpio regulator is part of linux. i.MX just provide control.
For the MSATA_DEVSLP, you need to consider about tie to PMIC_ON_REQ or PMIC_STBY_REQ depending on your design and your system design.
It is a customization scope, you need to figure out a way in your design.
mSATA differs from regular SATA only by form factor, so, basically, no driver code modification is required. The MSATA_DEVSLP, MSATA_PWR_EN signals you're talking about are non-standartized ones, so, they can be implemented by using any available GPIO.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi,Artur Petukhov:
thank u answer.
yes,
I want to make GPIO to control, but he did not offer the following section control pin design to me, how do I make him self-control action to 0 or 1, for example, I want to MSATA_PWR_EN control to GPIO_16 and low to high signal, how do I do?
Please help me,thanks.
So I just think it wrote dead. (for imx6q.dtsi code)
I want a similar code as follows:
imx6qdl-sabresd.dtsi:
reg_usb_h1_vbus: usb_h1_vbus {
compatible = "regulator-fixed";
regulator-name = "usb_h1_vbus";
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5000000>;
gpio = <&gpio3 31 0>; --> Control the way I want,control 0/1
enable-active-high;
};
imx6q.dtsi:
sata: sata@02200000 {
compatible = "fsl,imx6q-ahci";
reg = <0x02200000 0x4000>;
interrupts = <0 39 0x04>;
clocks = <&clks 154>, <&clks 187>, <&clks 105>;
clock-names = "sata", "sata_ref", "ahb";
status = "disabled";
};
You need to create a fixed regulator.
Assume you mentioned "written dead" is hard coding.
Where it is? What is MSATA_DEVSLP, MSATA_PWR_EN you mentioned in your hardware design?
If they are control by gpio, BSP is source code, you can modify anything you want.
BTW, MSATA_DEVSLP, MSATA_PWR_EN are the signals in the mSATA standard. Or they are just the name in you schematic. please confirm.
Hi,Biyong Sun:
yes,
I want to make GPIO to control, but he did not offer the following section control pin design to me, how do I make him self-control action to 0 or 1, for example, I want to MSATA_PWR_EN control to GPIO_16 and low to high signal, how do I do?
Please help me,thanks.
So I just think it wrote dead. (for imx6q.dtsi code)
I want a similar code as follows:
imx6qdl-sabresd.dtsi:
reg_usb_h1_vbus: usb_h1_vbus {
compatible = "regulator-fixed";
regulator-name = "usb_h1_vbus";
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5000000>;
gpio = <&gpio3 31 0>; --> Control the way I want,control 0/1
enable-active-high;
};
imx6q.dtsi:
sata: sata@02200000 {
compatible = "fsl,imx6q-ahci";
reg = <0x02200000 0x4000>;
interrupts = <0 39 0x04>;
clocks = <&clks 154>, <&clks 187>, <&clks 105>;
clock-names = "sata", "sata_ref", "ahb";
status = "disabled";
};
MSATA_DEVSLP(or call MSATA_DET), MSATA_PWR_EN is schematic name (cpu to issue).
MSATA_DEVSLP access Pin51 (mSATA interface).
MSATA_PWR_EN access another controller.
Mr Chen,
It is called fixed regulator. "compatible = "regulator-fixed";"
You should have device tree knowledge to read the dts file.
It's got nothing to do with sata. it is power supply.
For the MSATA_PWR_EN
Please follow binding guide Documentation\devicetree\bindings\regulator fixed-regulator.txt, add your gpio regulator.
And gpio regulator is part of linux. i.MX just provide control.
For the MSATA_DEVSLP, you need to consider about tie to PMIC_ON_REQ or PMIC_STBY_REQ depending on your design and your system design.
It is a customization scope, you need to figure out a way in your design.
Hi,Biyong Sun:
thank u answer.
I tried to do and if i have a problem, ask you again.
thanks!!!