Hi.
I'm running an image on an i.mx6D (build int Yocto).
The image is running from an emmc (Flash) which is around ~16Gb.
When I try to copy some files to the flash (via SSH) I get following problem:
/home/root/nodeJs/.......: No space left on device
I check the size of the disk with df -h, it there should be space left
Filesystem Size Used Avail Use% Mounted on
/dev/root 15G 9.5G 4.1G 70% /
devtmpfs 342M 4.0K 342M 1% /dev
tmpfs 502M 164K 502M 1% /run
tmpfs 502M 43M 460M 9% /var/volatile
/dev/mmcblk0p1 8.0M 8.0M 24K 100% /media/mmcblk0p1
Is there some setup I need to do to tell it that we are using 16 Gb disk when I compile or maybe some config file under /etc?
Thanks,
Niklas
已解决! 转到解答。
I found the problem.
Seems like I ran out of inodes (df -i, show Ifree = 0).
I had to remove some docker images (seems like there was an issue that inodes where not released after building docker images).
I found the problem.
Seems like I ran out of inodes (df -i, show Ifree = 0).
I had to remove some docker images (seems like there was an issue that inodes where not released after building docker images).