Hi everyone,
when i use uuu tool to update android9.0,there is one error happened as follow:
Wait for Known USB Device Appear...
>Start Cmd:CFG: FB: -vid 0x1fc9 -pid 0x0129
>Okay
New USB Device Attached at 7:6
7:6 >Start Cmd: FB: ucmd setenv fastboot_dev mmc
7:6 >Fail Bulk<W>:LIBUSB_ERROR_NOT_FOUND
<-[?25h
If you did not have fastboot.exe , then you should download it from below.
SDK Platform Tools release notes | Android Developers
Add the path of fastboot.exe into your PC "path environment variable ".
Then download P9.0.0_1.0.0_GA tools and source at Android OS for i.MX Applications Processors|NXP .
In GA release , there is one uuu_imx_android_flash.bat , you can try this bat file.
我也遇到了,同样的问题,请问有大神解决的吗?分享一下
we have the same problem, mark & wait for a solution.
E:\IMX8\android_p9.0.0_1.0.0-beta_image_8qmek>uuu.exe uuu-android-mx8qm-mek-emmc.lst
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.2.39-4-g219e333
Success 0 Failure 1
1/ 0 [ ]
1:6 1/21 [Bulk(W):LIBUSB_ERROR_NOT_FOU] FB: ucmd setenv fastboot_dev mmc
I am also getting the same issue with L4.14.78_1.0.0_MX8MQ release
Is there any way to flash into emmc other than Mfgtool & uuu
I am unable to flash into emmc through fastboot_imx_flashall.sh
getting the following
flash the file of partition-table.img to the partition of gpt
< waiting for device >
How can I enable my device (imx8mq) into fastboot mode
and when I tried to unlock the device I am getting following print
Usage:
fastboot <USB_controller>
- run as a fastboot usb device
Thank you very much,
Abhilash
Hello,
For the moment we do not have support for the L4.14.78 release, what I recommend you to use, is load the Yocto image through a Linux OS based machine with the command dd. For the moment, this is the easiest way that comes to my mind. Hope it can help you.
Best Regards,
Diego.
Hello,
Unfortunately, the Android 9 and the UUU tool are still in Beta mode, we do not have support until the software is officially released. I apologize for the inconveniences this could give to you.
Best Regards,
Diego.