I want to download the latest yocto resource Linux 5.10.9_ 1.0.0 according to https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat... : Linux 5.10.9_1.0.0 : " i.MX yocto project user's guide.pdf " , Synchronization failed !!!
That's what I did :
curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
... # get file repo from other community topic
# https://source.codeaurora.org/external/imx/imx-manifest/tree/README?h=imx-linux-gatesgarth
chmod a+x ~/bin/repo PATH=${PATH}:~/binexport REPO_URL='https://mirrors.tuna.tsinghua.edu.cn/git/git-repo' orexport REPO_URL='https://gerrit-googlesource.proxy.ustclug.org/git-repo'
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-gatesgarth -m imx-5.10.9-1.0.0.xml
repo sync
some error messages are as follows :
0 0 --:--:-- 0:02:00 --:--:-- 0\ncurl: (56) Unexpected EOF\n'
fsl-community-bsp-base:
fatal: unable to access 'https://github.com/Freescale/fsl-community-bsp-base/': gnutls_handshake() failed: The TLS connection was non-properly terminated.
meta-browser:
fatal: unable to access 'https://github.com/OSSystems/meta-browser/':Operation timed out after 300017 milliseconds with 0 out of 0 bytes received
fsl-community-bsp-base:
fatal: unable to access 'https://github.com/Freescale/fsl-community-bsp-base/': gnutls_handshake() failed: The TLS connection was non-properly terminated.
error: Cannot fetch fsl-community-bsp-base from https://github.com/Freescale/fsl-community-bsp-base
Fetching: 7% [2 jobs] (1/14) started meta-clang
meta-browser:
fatal: unable to access 'https://github.com/OSSystems/meta-browser/':gnutls_handshake() failed: The TLS connection was non-properly terminated.
...
meta-freescale:
fatal: unable to access 'https://github.com/Freescale/meta-freescale/': gnutls_handshake() failed: The TLS connection was non-properly terminated.
...
meta-qt5:
fatal: unable to access 'https://github.com/meta-qt5/meta-qt5/': Failed to connect to github.com port 443: 连接超时
meta-openembedded:
fatal: unable to access 'https://github.com/openembedded/meta-openembedded/': gnutls_handshake() failed: The TLS connection was non-properly terminated.
meta-openembedded:
fatal: unable to access 'https://github.com/openembedded/meta-openembedded/': gnutls_handshake() failed: The TLS connection was non-properly terminated.
...
and so on
...
The result is not 100% synchronization
how i can do now ?
Hello raotianxiang,
You must fix your proxy issues, that error is common issue with proxie not from yocto.
Regards
@Bio_TICFSL i am also facing the same issue, so how to resolve this proxy , because i have not set any proxy and where to check it
i have followed the IMXLXYOCTOUG i.MX Yocto Project User's Guide Rev. LF5.10.9_1.0.0 — 12 April 2021 . i am working on : Rugged Board , PhyCore - i.MX6 UL (MCIMX6G2CVM05AB) . Host machine is ubuntu18.4
i executed the commands as mentioned below and the error it shows::
--------------------------------------------------------------------------------------------------------------------------------------
r@dell:~/bin/imx-yocto-bsp$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-gatesgarth -m imx-5.10.9-1.0.0.xml
fatal: Cannot get https://gerrit.googlesource.com/git-repo/clone.bundle
fatal: error [SSL: CERTIFICATE_VERIFY_FAILED] certificate verify failed (_ssl.c:727)
r@dell:~/bin/imx-yocto-bsp$
--------------------------------------------------------------------------------------------------------------------------------------
When I built imx-image-full, I found that qtwangland always failed to compile.
lib drm ?
I had cleanall-ed them and rebuild , but no effect