enable CAN in i.MX6SoloX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

enable CAN in i.MX6SoloX

1,288 Views
jibin1246
Contributor II

How to enable CAN in i.MX6SoloX ?

0 Kudos
Reply
1 Reply

1,103 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

The Linux BSP already includes FlexCAN drivers for i.MX6SX (mounted as a network interface). In order to check the driver overview, hardware and software operation, source code structure and menu configuration options please refer to Chapter 37 “FlexCAN Driver” of the “i.MX Linux® Reference Manual” document (attached).

It may be also required to change the Device Tree file, as there could be some pin conflicts. Please take a look at Table 10 “Supported features” of the “i.MX Linux® Release Notes” document (also attached).

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------