Dear all,
We want to use eMMC memory with pSLC mode with i.MX25.
In this case, it is necessary for [156]PARTITIONS_ATTRIBUTE of Extended CSD Register to be programed
However, the eMMC I/F of i.MX25 is Specification Version 4.2.
We understand that Version 4.2 does not support this operation.
Can eMMC of i.MX25 support pSLC mode by software modification?
(Can [156]PARTITIONS_ATTRIBUTE of Extended CSD Register be programed by software?)
May I have advice?
Best Regards,
Yuuki
解決済! 解決策の投稿を見る。
Hi Yuuki
>(Can [156]PARTITIONS_ATTRIBUTE of Extended CSD Register be programed by software?)
yes, i.MX25 SDHC support such operation using CMD6 and this is described in
Table 23-30. Commands for MMC/SD/SDIO/CE-ATA Cards i.MX25 Reference Manual (rev.2, 1/2011)
http://www.freescale.com/files/dsp/doc/ref_manual/IMX25RM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuuki
>(Can [156]PARTITIONS_ATTRIBUTE of Extended CSD Register be programed by software?)
yes, i.MX25 SDHC support such operation using CMD6 and this is described in
Table 23-30. Commands for MMC/SD/SDIO/CE-ATA Cards i.MX25 Reference Manual (rev.2, 1/2011)
http://www.freescale.com/files/dsp/doc/ref_manual/IMX25RM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------