eMMC compatibility list (iMX23)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC compatibility list (iMX23)

1,728 Views
rolfheimerdinge
Contributor II

Hi,

is there any compatibility list of eMMC devices vs processor?

We use iMX23, and our eMMC (Toshiba THGBM 4 G 4 D 1 HBAIR) has EOL.

Would be also great if you name a working eMMC with iMX23.

Thanks,

Rolf Heimerdinger

Labels (1)
0 Kudos
Reply
1 Reply

858 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rolf

I am afraid there is no such list.

Regarding supported SD/MMC formal answer is given in

sect.35.7 SD/MMC Boot Mode IMX23RM

SD/MMC boot mode supports booting from SD/MMC cards adhering to the following specifications:

• iNand Product Manual, Version 2.1

• SD Specifications, Part 1, Physical Layer Specification, Version 1.10

• SD Specifications, Part 1, Physical Layer Specifications, Version 2.0 Draft

• MultiMediaCard System Specification, Version 4.1

• MultiMediaCard System Specification, Version 4.2

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply