eMMC Flash partition READ-WRITE from Read Only

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC Flash partition READ-WRITE from Read Only

1,521 Views
mselvara82
Contributor I

Please find below details and query.

~ # fdisk -l

Disk /dev/mmcblk0: 116 MB, 116523008 bytes
4 heads, 16 sectors/track, 3556 cylinders
Units = cylinders of 64 * 512 = 32768 bytes

Device Boot Start End Blocks Id System
/dev/mmcblk0p1 73 200 4096 83 Linux
/dev/mmcblk0p2 201 328 4096 83 Linux
/dev/mmcblk0p3 329 872 17408 83 Linux
/dev/mmcblk0p4 873 3556 85888 5 Extended
/dev/mmcblk0p5 877 1420 17408 83 Linux
/dev/mmcblk0p6 1425 1488 2048 83 Linux
/dev/mmcblk0p7 1493 1556 2048 83 Linux
/dev/mmcblk0p8 1573 1668 3072 83 Linux
/dev/mmcblk0p9 1673 1768 3072 83 Linux
/dev/mmcblk0p10 1773 1836 2048 83 Linux
/dev/mmcblk0p11 1841 1904 2048 83 Linux
/dev/mmcblk0p12 1909 2196 9216 83 Linux
/dev/mmcblk0p13 2201 2488 9216 83 Linux
/dev/mmcblk0p14 2493 2940 14336 83 Linux
/dev/mmcblk0p15 2945 3392 14336 83 Linux

The Partition /dev/mmcblk0p13 which is used for rootfs. But it is in Read-Only mode.

For debugging purpose, I need to change Read-Write permission for /dev/mmcblk0p13.

Can you please share the procedure to convert to Read-Write?

The Partition /dev/mmcblk0p13 which is based on squashfs.

~ # mount
/dev/root on / type squashfs (ro,relatime)


Please share your inputs.

0 Kudos
Reply
0 Replies