eMMC Booting Fail in i.MX6S on Low Temperature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC Booting Fail in i.MX6S on Low Temperature

1,759 Views
erickang
Contributor II

Dear All,

I'm using the i.MX6S with eMMC and Android JB 4.3.

 

But the board was not booted in Low Temperature with below messages.

Could you give me any guidance for this issue?

For whole log message, refer to attached file.

 

** Can't read partition table on 3:0 **

booti: device don't have such partition:boot

fastboot is in init......flash target is MMC:3

** Can't read partition table on 3:0 **

Bad partition index:1 for partition:boot

** Can't read partition table on 3:0 **

Bad partition index:2 for partition:recovery

** Can't read partition table on 3:0 **

Bad partition index:5 for partition:system

wait usb cable into the connector!

 

Best Regards,

Eric.

Original Attachment has been moved to: eMMC_Partition.Detection.Fail.log.txt.zip

Labels (3)
0 Kudos
Reply
1 Reply

853 Views
igorpadykov
NXP Employee
NXP Employee

Hi Eric

I would suggest to run SDK (it has block read/write test)

and check if issue will present. Failures at low temperatures

may mean that drive strength i.MX6 and eMMC pads is too strong,

one can try to decrease it, example can be found below

https://community.freescale.com/thread/332110

also one can try other eMMC, since these chips may differ in

its driver strength characteristics.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply