eIQ enable on MX8QXPMEK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eIQ enable on MX8QXPMEK

1,701 次查看
mahesh93
Contributor III

Hi, I am using L5.4.24-2.1.0 BSP to enable eIQ with GPU on i.MX8QXPMEK (B0)

I have some questions..

1. is L5.4.24-2.1.0 BSP comes with eIQ ? i see only one demo multimedia image on website

https://www.nxp.com/webapp/Download?colCode=L5.4.24_2.1.0_MX8QXPB0&appType=license

2. How i can use GPU with this BSP ?

0 项奖励
10 回复数

1,689 次查看
joanxie
NXP TechSupport
NXP TechSupport

yes, 5.4.24 supports it, you can find the source code as below:

"https://community.nxp.com/t5/eIQ-Machine-Learning-Software/eIQ-Download-Information/ta-p/1111438"

 

how to use it you can refer to the document:

"https://www.nxp.com/docs/en/nxp/user-guides/UM11226.pdf"

0 项奖励

1,679 次查看
mahesh93
Contributor III

Thanks joanxie, 

       after flashing BSP https://www.nxp.com/webapp/Download?colCode=L5.4.24_2.1.0_MX8QXPB0&appType=license

The board is up but i don't see "tensorflow-lite-2.1.0/examples" in path "/usr/bin/"

am i missing anything while flashing or configuration ?

0 项奖励

1,652 次查看
joanxie
NXP TechSupport
NXP TechSupport

try to use the latest version, 5.10.9 or 5.4.70

 

0 项奖励

1,647 次查看
mahesh93
Contributor III

Hi, when i run bitbake imx-image-full somewhere in middle 

I get this error.........

mahesh93_0-1619435145626.png

0 项奖励

1,645 次查看
joanxie
NXP TechSupport
NXP TechSupport

this is your network issue, delete this package and build again, use the command like "bitbake -c cleansstate libarchive-native" then bitabke libarchive-native

 

0 项奖励

1,625 次查看
mahesh93
Contributor III

Hi, 

    Is it possible to get built image with this configurations

$ DISTRO=fsl-imx-xwayland MACHINE=imx8qxpmek source imx-setup-release.sh -b build-xwayland
$ bitbake imx-image-full

It is taking huge time and space to build

标记 (1)
0 项奖励

1,611 次查看
joanxie
NXP TechSupport
NXP TechSupport

you can try to download demo images from the official website, if the name doesn't include c0, should available for B0, like "imx-boot-imx8qxpmek-sd.bin-flash" is for B0, and "imx-boot-imx8qxpc0mek-sd.bin-flash" is for C0, you can try it

0 项奖励

1,605 次查看
mahesh93
Contributor III

okay thanks, i got bootloader, But  where will i get <rootfs> ? can i use same of C0 ?

0 项奖励

1,595 次查看
joanxie
NXP TechSupport
NXP TechSupport

roofs is maybe default for C0, maybe you need to replace some files, you can download to the SD card and open it to check them

 

0 项奖励

1,652 次查看
mahesh93
Contributor III

Hi Joanxie, i used 5.4.70 but it is for C0 variant of board, What i have is B0....so it is not booting...let me try other you mentioned Thanks

0 项奖励