Hi ,
i have imx6 base board(Udoo quad) with android 4.3
I have a problem with resistive egalax touchscreen.
It's fliped up side down / swap y .
Question is how to calibrate the touchscreen? the program witch is installed on android for calibration, not recognize my touchscreen.
Where i can find the file witch have the settings for touchscreen?
Thank you.
Sorry for my English.
Nobody? :smileysad:
Is this so hard for you guys?
Maybe this can help a litlle.
root@udoo:/ # su -- getevent -lp /dev/input/event0
add device 1: /dev/input/event0
name: "eGalax Inc. USB TouchController"
events:
KEY (0001): BTN_TOUCH
ABS (0003): ABS_X : value 1322, min 0, max 2047, fuzz 0, flat 0, resolution 0
ABS_Y : value 1119, min 0, max 2047, fuzz 0, flat 0, resolution 0
input props:
<none>
root@udoo:/ #