Tool for performance analysis for i.MX6Q Sabre Lite Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tool for performance analysis for i.MX6Q Sabre Lite Board

572 Views
douglassantos
Contributor I

Hi all,

I'm using the i.MX6Q Sabre Lite Board to test some algorithms and would like to know if there is any tool that can assist me in collecting data, such as processing time and the resources used (CPU, GPU).

Thanks in advance,

Douglas

Labels (1)
0 Kudos
Reply
1 Reply

398 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Douglas,

I can only recommend that you use the TOP linux command so you can get the information that you are trying to accomplish, here is a link, that can help:

Unbelievable ! 30 Linux TOP Command Examples With Screenshots

For the GPU you can use the VProfiler, that it is a tool from the Vivante SDK,  you can download it from the following link:

I.MX_6_VIVANTE_VDK_150_TOOLS , just a little advise, this is tool it is made for the Freescale BSP since you are using the SABRE Lite board from Nitrogen. You need to check if the GPU it is enable in your kernel.

saludos

0 Kudos
Reply