don't run configure as root , set FORCE_UNSAFE_CONFIGURE=1 in environment to bypass this check

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

don't run configure as root , set FORCE_UNSAFE_CONFIGURE=1 in environment to bypass this check

2,150 次查看
shivam_rawat
Contributor II

i have followed the IMXLXYOCTOUG i.MX Yocto Project User's Guide Rev. LF5.10.9_1.0.0 — 12 April 2021 . i have executed the command bitbake imx-image-multimedia and got the error mentioned below .  
i am working on : Rugged Board ,  PhyCore - i.MX6 UL (MCIMX6G2CVM05AB) .
host machine is ubuntu18.4 

i executed the commands as mentioned below:
$  repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-gatesgarth -m imx-5.10.9-1.0.0.xml
$  repo sync

$ DISTRO=fsl-imx-x11 MACHINE=imx6ulevk source imx-setup-release.sh -b ./fsl_build_x11
$  bitbake imx-image-multimedia
______________________________________________________________________

 

 

root@dell:~/bin/imx-yocto-bsp/fsl_build_x11# bitbake imx-image-multimedia
Loading cache: 100% |##################################################################################################################| Time: 0:00:01
Loaded 4847 entries from dependency cache.
Parsing recipes: 100% |################################################################################################################| Time: 0:00:02
Parsing of 3281 .bb files complete (3280 cached, 1 parsed). 4848 targets, 317 skipped, 1 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.48.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-18.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6ulevk"
DISTRO = "fsl-imx-x11"
DISTRO_VERSION = "5.10-gatesgarth"
TUNE_FEATURES = "arm vfp cortexa7 neon thumb callconvention-hard"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:943ef2fad8428f002850e3655a3312e13d0dcb2c"
meta-oe
meta-multimedia
meta-python = "HEAD:ac4ccd2fbbb599d75ca4051911fcbaca39dbe6d7"
meta-freescale = "HEAD:41d4f625c6db7a778f0f9a735c2cb48e023bc49b"
meta-freescale-3rdparty = "HEAD:b85d08a55cb833bfc4e8b5034ff804286c67620e"
meta-freescale-distro = "HEAD:11be3f01962df8436c5c7b0d61cd3dbd1b872905"
meta-bsp
meta-sdk
meta-ml = "HEAD:478d788fc1ecb4783a2702752a61f1035fe9ab9f"
meta-nxp-demo-experience = "HEAD:b5c3d6c3e91a3914ae7a3fabec86295dbb00057d"
meta-browser = "HEAD:ee3be3b5986a4aa0e73df2204a625ae1fe5df37e"
meta-rust = "HEAD:53bfa324891966a2daf5d36dc13d4a43725aebed"
meta-clang = "HEAD:61faae011fb95712064f2c58abe6293f0daeeab5"
meta-gnome
meta-networking
meta-filesystems = "HEAD:ac4ccd2fbbb599d75ca4051911fcbaca39dbe6d7"
meta-qt5 = "HEAD:8d5672cc6ca327576a814d35dfb5d59ab24043cb"
meta-python2 = "HEAD:c43c29e57f16af4e77441b201855321fbd546661"

Initialising tasks: 100% |#############################################################################################################| Time: 0:00:07
Sstate summary: Wanted 2072 Found 0 Missed 2072 Current 1490 (0% match, 41% complete)
NOTE: Executing Tasks
ERROR: coreutils-native-8.32-r0 do_configure: configure failed
ERROR: coreutils-native-8.32-r0 do_configure: Execution of '/root/bin/imx-yocto-bsp/fsl_build_x11/tmp/work/x86_64-linux/coreutils-native/8.32-r0/temp/run.do_configure.17875' failed with exit code 1:
automake (GNU automake) 1.16.2
Copyright (C) 2020 Free Software Foundation, Inc.
License GPLv2+: GNU GPL version 2 or later <https://gnu.org/licenses/gpl-2.0.html>
This is free software: you are free to change and redistribute it.
There is NO WARRANTY, to the extent permitted by law.

Written by Tom Tromey <tromey@redhat.com>
and Alexandre Duret-Lutz <adl@gnu.org>.
AUTOV is 1.16
autoreconf: Entering directory `.'
autoreconf: running: aclocal --system-acdir=/root/bin/imx-yocto-bsp/fsl_build_x11/tmp/work/x86_64-linux/coreutils-native/8.32-r0/recipe-sysroot-native/usr/share/aclocal/ --automake-acdir=/root/bin/imx-yocto-bsp/fsl_build_x11/tmp/work/x86_64-linux/coreutils-native/8.32-r0/recipe-sysroot-native/usr/share/aclocal-1.16 -I ./m4 --force -I m4
autoreconf: configure.ac: tracing

.

.

.

.

.

.

| checking for mkfifo... yes
| checking whether mkfifo rejects trailing slashes... yes
| checking whether mknod can create fifo without root privileges... configure: error: in `/root/bin/imx-yocto-bsp/fsl_build_x11/tmp/work/x86_64-linux/coreutils-native/8.32-r0/build':
| configure: error: you should not run configure as root (set FORCE_UNSAFE_CONFIGURE=1 in environment to bypass this check)
| See `config.log' for more details
| WARNING: exit code 1 from a shell command.
|
ERROR: Task (virtual:native:/root/bin/imx-yocto-bsp/sources/poky/meta/recipes-core/coreutils/coreutils_8.32.bb:do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 5405 tasks of which 5363 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
virtual:native:/root/bin/imx-yocto-bsp/sources/poky/meta/recipes-core/coreutils/coreutils_8.32.bb:do_configure
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
root@dell:~/bin/imx-yocto-bsp/fsl_build_x11#


+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
--------------------------------------------------------------------------------------------------------------------------------

i did "export  FORCE_UNSAFE_CONFIGURE=1 " on the same shell but still got the same error again

 

标签 (3)
0 项奖励
回复
0 回复数