Good Morning,
on trying to compile a custom make-file-based package ("libxbee"), I get an error while the do_package routine is running. My board is iMX6 wandboard-quad and I am using the dora-branch.
ERROR: objcopy failed with exit code 256 (cmd was 'arm-poky-linux-gnueabi-objcopy' --add-gnu-debuglink='/..../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxbee/3-r2/package/usr/lib/.debug/libxbee.so.3.0.10' '/..../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxbee/3-r2/package/usr/lib/libxbee.so.3.0.10'):
arm-poky-linux-gnueabi-objcopy:/..../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxbee/3-r2/package/usr/lib/stB6ee1m: cannot create debug link section `/..../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxbee/3-r2/package/usr/lib/.debug/libxbee.so.3.0.10': Invalid operation
ERROR: Function failed: split_and_strip_files
ERROR: Logfile of failure stored in: /..../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxbee/3-r2/temp/log.do_package.3126
ERROR: Task 516 (/..../sources/meta-wvsnp-pkgs/recipes-libxbee/libxbee/libxbee_3.bb, do_package) failed with exit code '1'
I had some troubles to get it compiling, but these steps are running through smoothly now. But I cannot figure out what exactly fails during the packaging-process. To be honest, I can't even tell what the process is doing in detail (other than, you know, "packaging").
If you need it, here is my recipe file for it:
DESCRIPTION = "A C/C++ library to aid the use of Digi XBee radios in API mode."
SECTION = "base"
HOMEPAGE = "http://code.google.com/p/libxbee/"
LICENSE = "GPLv2+"
LIC_FILES_CHKSUM = "file://COPYING;md5=d32239bcb673463ab874e80d47fae504"
SRC_URI = "git://github.com/attie/libxbee3.git;protocol=git"
SRCREV = "aad1fce3864eccc80a003b3b93010e6f56bb87dd"
S = "${WORKDIR}/git/"
PR = "r1"
do_configure() {
oe_runmake configure
}
do_compile() {
oe_runmake all
}
do_install () {
mkdir -p ${D}/usr/share/man/man3
oe_runmake install SYS_ROOT=${D}
}
Does anyone have an idea?
Thanks,
Lukas.
已解决! 转到解答。
Hi everyone,
Thanks for your help, I got it running finally. I played around with autotools and the EXTRA_OEMAKE variable, but it did not seem to ehlp.
My solution seemed to be to add $libdir to the FILES_{$PN} variable and disable stripping according to Re: [yocto] How to pack non striped valgrind image into squashfs image:
If you want the binaries not to be stripped, try
adding INHIBIT_PACKAGE_STRIP = "1" to valgrind recipe.
This will disable stripping the binaries as you have mentioned.
Here's my running recipe:
DESCRIPTION = "A C/C++ library to aid the use of Digi XBee radios in API mode."
SECTION = "base"
HOMEPAGE = "http://code.google.com/p/libxbee/"
LICENSE = "LGPLv3"
LIC_FILES_CHKSUM = "file://COPYING;md5=d32239bcb673463ab874e80d47fae504"
SRC_URI = "git://github.com/attie/libxbee3.git;protocol=git"
SRCREV = "aad1fce3864eccc80a003b3b93010e6f56bb87dd"
S = "${WORKDIR}/git/"
PR = "r1"
INHIBIT_PACKAGE_STRIP = "1"
FILES_${PN} += "${libdir}/"
do_configure() {
echo ${libdir}
oe_runmake configure
}
do_compile() {
oe_runmake all
}
do_install () {
mkdir -p ${D}/usr/share/man/man3
oe_runmake install SYS_ROOT=${D}
}
Hi everyone,
Thanks for your help, I got it running finally. I played around with autotools and the EXTRA_OEMAKE variable, but it did not seem to ehlp.
My solution seemed to be to add $libdir to the FILES_{$PN} variable and disable stripping according to Re: [yocto] How to pack non striped valgrind image into squashfs image:
If you want the binaries not to be stripped, try
adding INHIBIT_PACKAGE_STRIP = "1" to valgrind recipe.
This will disable stripping the binaries as you have mentioned.
Here's my running recipe:
DESCRIPTION = "A C/C++ library to aid the use of Digi XBee radios in API mode."
SECTION = "base"
HOMEPAGE = "http://code.google.com/p/libxbee/"
LICENSE = "LGPLv3"
LIC_FILES_CHKSUM = "file://COPYING;md5=d32239bcb673463ab874e80d47fae504"
SRC_URI = "git://github.com/attie/libxbee3.git;protocol=git"
SRCREV = "aad1fce3864eccc80a003b3b93010e6f56bb87dd"
S = "${WORKDIR}/git/"
PR = "r1"
INHIBIT_PACKAGE_STRIP = "1"
FILES_${PN} += "${libdir}/"
do_configure() {
echo ${libdir}
oe_runmake configure
}
do_compile() {
oe_runmake all
}
do_install () {
mkdir -p ${D}/usr/share/man/man3
oe_runmake install SYS_ROOT=${D}
}
Hi Lukas,
Sorry to hear you're having issues.
I also noticed that you've put the licence as GPLv2+.
It's actually licensed using LGPLv3 if that's an option in your build system.
I hope this helps,
Attie
Hi Lukas,
if you are using autotools for the compilation (alias make), you should inherit the class, so first try your recipe with
DESCRIPTION = "A C/C++ library to aid the use of Digi XBee radios in API mode."
SECTION = "base"
HOMEPAGE = "http://code.google.com/p/libxbee/"
LICENSE = "GPLv2+"
LIC_FILES_CHKSUM = "file://COPYING;md5=d32239bcb673463ab874e80d47fae504"
SRC_URI = "git://github.com/attie/libxbee3.git;protocol=git"
SRCREV = "aad1fce3864eccc80a003b3b93010e6f56bb87dd"
S = "${WORKDIR}/git/"
PR = "r1"
inherit autotools
Hi,
autotools won't help in my case, or I cannot utilise it. The installation (do_install) process will fail, if I do not use my custom do_install routine..
ERROR: Function failed: do_install (log file is located at /.../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxbee/3-r2/temp/log.do_install.6196)
ERROR: Logfile of failure stored in: /.../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxbee/3-r2/temp/log.do_install.6196
Log data follows:
| DEBUG: SITE files ['endian-little', 'bit-32', 'arm-common', 'common-linux', 'common-glibc', 'arm-linux', 'arm-linux-gnueabi', 'common']
| DEBUG: Executing shell function do_install
| NOTE: make -j 4 SYS_ROOT=/.../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxbee/3-r2/image DESTDIR=/.../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxbee/3-r2/image install
| make: *** No rule to make target `/.../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxbee/3-r2/image.dir', needed by `/.../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxbee/3-r2/image/libxbee.so.3.0.10'. Stop.
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_install (log file is located at /.../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxbee/3-r2/temp/log.do_install.6196)
ERROR: Task 508 (/.../sources/meta-wvsnp-pkgs/recipes-libxbee/libxbee/libxbee_3.bb, do_install) failed with exit code '1'
On leaving the custom do_install but inheriting from autotools, will still produce the same error as in the first posting.
You may post this question to the meta-freescale list. Also, there is an example on this section http://www.yoctoproject.org/docs/current/dev-manual/dev-manual.html#usingpoky-extend-addpkg-autotool...
Leo