demo image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

demo image

3,057件の閲覧回数
sachusanal
Contributor III

Hai Sir ,

Could you please give me the  Demo image (prebuit imag ) for Mx6qsabresd board (evaluation kit).

ラベル(1)
0 件の賞賛
返信
25 返答(返信)

2,455件の閲覧回数
sachusanal
Contributor III

could u please share me mx6q sabresd board  .sd card image.

in this download only contain imx6soloboard image

please reply its urgent one

0 件の賞賛
返信

2,455件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please use

\L3.14.28_1.0.0_ga_images_MX6.tar\L3.14.28_1.0.0_ga_images_MX6\fsl-image-gui-x11-imx6qdlsolo.sdcard

in the mentioned package.

Regards,

Yuri.

0 件の賞賛
返信

2,455件の閲覧回数
sachusanal
Contributor III

Hai yuri ,

I created sdb1 partition on Sd card. because at the starting sd card have no partition .

then i copied that solo image to sd card. but it is not working the imx6Qsabresd  evaluation kit.

please reply me.

it's urgent one

0 件の賞賛
返信

2,455件の閲覧回数
Yuri
NXP Employee
NXP Employee

Have You used the Linux host to deploy the image with the following command ?

$ sudo dd if= fsl-image-qt5-x11-imx6qdlsolo.sdcard of=/dev/sdb1 bs=1M

After that insert the SD card to the board and power on ?

Are Your boot configuration correct ? Please check it - SD3 boot.

Regards,

Yuri.

0 件の賞賛
返信

2,454件の閲覧回数
ruihongfeng-b36
NXP TechSupport
NXP TechSupport

Hi Yuri,

I did some test and tried if I can post on community.

Please ignore or reject my content.

Annie

0 件の賞賛
返信

2,454件の閲覧回数
sachusanal
Contributor III

could u please share me the working "fsl-image-gui-x11-imx6qdlsolo.sdcard

0 件の賞賛
返信

2,454件の閲覧回数
sachusanal
Contributor III

Hai yuri ,

Thanks for the response

I have one doubt when i mount my SD card

i listed out drivers in  ls /dev

i can find only sdb

sdb is my SD card

there is no sdb1 when i am copying  this image by using this command sudo dd if= fsl-image-qt5-x11-imx6qdlsolo.sdcard of=/dev/sdb1 bs=1M

through this command sdb1 partition created in disk or device ?

0 件の賞賛
返信

2,454件の閲覧回数
sachusanal
Contributor III

hai yuri its working...

thanks..

let me know in this demo image contain any qt application . ?

could u please tell me the location of the qt application?

please tell meee

0 件の賞賛
返信

2,454件の閲覧回数
Yuri
NXP Employee
NXP Employee

The package on the Web (fsl-L3.14.28_1.0.0_iMX6qdls_Bundle.tar.gz) contains

"fsl-image-qt5-x11-imx6qdlsolo.sdcard"

Regards,

Yuri.

0 件の賞賛
返信

2,455件の閲覧回数
sachusanal
Contributor III

Hai Yuri ,

I copied the image by using this command  sudo dd if= fsl-image-qt5-x11-imx6qdlsolo.sdcard of=/dev/sdb1 bs=1M

after that the SD card is put in board. i didnt passs any boot arguemts the boot loader log is also not shown in teraterm

my Evaluation kit is MCIMX6Q-SDP

please help me

its an urgent issue

0 件の賞賛
返信

2,455件の閲覧回数
sachusanal
Contributor III

hai yuri ,

I copied the image by using sudo dd if= fsl-image-qt5-x11-imx6qdlsolo.sdcard of=/dev/sdb1 bs=1M this command.

but it is not loading ,uboot also not loading ...

please help me

0 件の賞賛
返信

2,454件の閲覧回数
Yuri
NXP Employee
NXP Employee

Sorry, the /dev/sdb1 - this is a misprint. The whole device should be used - /dev/sdb

Regards,

Yuri.

0 件の賞賛
返信

2,455件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Just tried "fsl-image-gui-x11-imx6qdlsolo.sdcard" from the Web - it is working

on my board.

Regards,

Yuri.

0 件の賞賛
返信

2,455件の閲覧回数
sachusanal
Contributor III

let me know u tried out in MX6Qsabresd board

0 件の賞賛
返信

2,455件の閲覧回数
Yuri
NXP Employee
NXP Employee

What is Your boot configuration (SW6) ?

Regards,

Yuri.

0 件の賞賛
返信

2,455件の閲覧回数
sachusanal
Contributor III

pastedImage_0.png

0 件の賞賛
返信

2,455件の閲覧回数
Yuri
NXP Employee
NXP Employee

Is Your board working ?
Can You use MFG with the board ?

Regards,

Yuri.

0 件の賞賛
返信

2,455件の閲覧回数
sachusanal
Contributor III

my board is working.

Now i  download android prebuilt image by using MFG tool. this is working properly in my board

could u please help me to flash the image by using mfg tool  give me the mfgtool image ,mfgtool for downloading the prebuilt image to my board

0 件の賞賛
返信

2,455件の閲覧回数
ruihongfeng-b36
NXP TechSupport
NXP TechSupport

test

0 件の賞賛
返信

2,455件の閲覧回数
sachusanal
Contributor III

Hai Ruihong ,

I have tested with these two images in mx6qsabresd evaluation kit which purchased from freescale ( fsl-image-qt5-x11-imx6qdlsolo.sdcard ,fsl-image-gui-x11-imx6qdlsolo.sdcard) both the images are not booting imx6qsabresd board evaluation kit.

could u please help me to solve this issue

could u please give me the exact image for imx6qsabrsd board

0 件の賞賛
返信