Hi NXPs,
My name is Toan. I am using iMX6ULEVK with kernel 4.14.98. Currently, I want to read video from OV5640 camera on python3 with OpenCV by Gstreamer. And I'm using:
camera = cv2.VideoCapture("imxv4l2src device=/dev/video1 ! video/x-raw-yuv format=YUYV, width=1280 , height=720 , framerate=(fraction)30/1 ! appsink")
But I got this error:
Traceback (most recent call last):
File "streamOV5640.py", line 14, in <module>
cv2.imshow("Streaming.",frame)
cv2.error: OpenCV(4.0.1) /usr/src/debug/opencv/4.0.1.imx-r0/git/modules/imgproc/src/color.hpp:259: error: (-2:Unspecified error) in function 'cv::CvtHelper<VScn, VDcn, VDepth, sizePolicy>::CvtHelper(cv::InputArray, cv::OutputArray, int) [with VScn = cv::Set<3, 4>; VDcn = cv::Set<3, 4>; VDepth = cv::Set<0, 2, 5>; cv::SizePolicy sizePolicy = (cv::SizePolicy)2; cv::InputArray = const cv::_InputArray&; cv::OutputArray = const cv::_OutputArray&]'
> Invalid number of channels in input image:
> 'VScn::contains(scn)'
> where
> 'scn' is 2
I found that output image is only 2 channels colors:
[[[141 124]
[142 127]
[142 124]
...
How does its happen ? I never met this case before. Did I miss somethings and how can I fix this ?
Thank you so much,
Toan
Hi Bio_TICFSL,
Thanks for you response. I tried this but FPS is about 7.5 FPS. It's quite low so I finding other solution. I used gst-launch-1.0 command can reach at 30 FPS. It's so perfect if I get the same thing with OpenCV-Python. DO you have some ideas ?
Thank you so much,
Toan