core-image-* (minimal) with cmake

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

core-image-* (minimal) with cmake

893 Views
erikraynolds
Contributor III

I am building core-image-minimal where I wanna include cmake but by building it with local.conf configured to include cmake it's not enabled and present on image

MACHINE ??= 'imx8qmmek'

DISTRO ?= 'fsl-imx-xwayland'
PACKAGE_CLASSES ?= "package_rpm"
EXTRA_IMAGE_FEATURES ?= "debug-tweaks"
USER_CLASSES ?= "buildstats image-mklibs image-prelink"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS = "\
STOPTASKS,${TMPDIR},1G,100K \
STOPTASKS,${DL_DIR},1G,100K \
STOPTASKS,${SSTATE_DIR},1G,100K \
STOPTASKS,/tmp,100M,100K \
ABORT,${TMPDIR},100M,1K \
ABORT,${DL_DIR},100M,1K \
ABORT,${SSTATE_DIR},100M,1K \
ABORT,/tmp,10M,1K"
PACKAGECONFIG_append_pn-qemu-native = " sdl"
PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"
CONF_VERSION = "1"

DL_DIR ?= "${BSPDIR}/downloads/"
ACCEPT_FSL_EULA = "1"

EXTRA_IMAGE_FEATURES_append = " debug-tweaks eclipse-debug dev-pkgs tools-debug tools-sdk ssh-server-openssh"
TOOLCHAIN_HOST_TASK_append = " nativesdk-cmake nativesdk-make"

IMAGE_INSTALL_append = " cmake"
IMAGE_INSTALL_append = " openssh-sftp-server tcf-agent sshfs-fuse"
IMAGE_INSTALL_append = " net-tools iputils dhcpcd"

How to get cmake on core-image-minimal?

Tags (2)
0 Kudos
Reply
1 Reply

766 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Erik Raynolds,

The steps for adding cmake look correct. Have you checked on the bitbake log that this task was run correctly? I haven’t tested it but this would install cmake but not configure it so you would need to setup the toolchain, paths and flags in order to use cmake.

Regards,

0 Kudos
Reply