Hello,
In linux device tree there is configuration for sdio clock-frequency:
&usdhc2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc2_2>;
no-1-8-v;
bus-width = <4>;
clock-frequency = <40000000>;
max-frequency = <40000000>;
keep-power-in-suspend;
enable-sdio-wakeup;
status = "okay";
};
But in u-boot I don't find such configuration, so I wander, how is it that u-boot can manage working with sdio in a slower rate, while linux need to be configured for that rate in device tree ?
Thank you,
Ran
解決済! 解決策の投稿を見る。
this may be due to drive strength and associated with it
signal integrity issues, in *dts file one can check for example:
pinctrl_usdhc3: usdhc3grp {
fsl,pins = <
MX6QDL_PAD_SD3_CMD__SD3_CMD 0x17059
MX6QDL_PAD_SD3_CLK__SD3_CLK 0x10059
which corresponds to register IOMUXC_SW_PAD_CTL_PAD_SD3_CLK,
one can tweak DSE settings
Best regards
igor
Hi Ran
seems uboot uses rom boot usdhc settings described in
sect.8.5.3.1 Expansion Device eFUSE Configuration i.MX6DQ
Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you,
I have a strange issue where I can access mmc from u-boot (mmc commands), but not from linux.
Not sure yet, why. It is a new board design. older design worked very well.
If the failure was both in u-boot and linux, it was easier, and we could tell is it a HW issue.
But since from u-boot is seems to work, we are not sure.
Regards,
Ran
this may be due to drive strength and associated with it
signal integrity issues, in *dts file one can check for example:
pinctrl_usdhc3: usdhc3grp {
fsl,pins = <
MX6QDL_PAD_SD3_CMD__SD3_CMD 0x17059
MX6QDL_PAD_SD3_CLK__SD3_CLK 0x10059
which corresponds to register IOMUXC_SW_PAD_CTL_PAD_SD3_CLK,
one can tweak DSE settings
Best regards
igor