chrome on imx6 dual lite

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

chrome on imx6 dual lite

1,646 次查看
ranwainstein
Contributor I

Hi, 

We are running chromium on  imx6 duallite , the performance are not good. 

CPU average at 50-80 % load, and overall user experience is not good. 

when typing "chrome://gpu" we see that HW accelerator is enabled ( Vivante 880 ) .

 Our desktop is LXQT ( QT5 Based ) .

1. Is there a know issues with chrome in imx6 processors ? 

2. Can you describe the steps for adding chrome to #i.mx6 yocto in order to get best graphics performance ? 

Thanks, 

Ran 

0 项奖励
回复
1 回复

785 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  You may try the recent NXP Linux BSP.  Look at section 5.6.6 (Chromium Browser on X11,

XWayland, and Wayland) of "i.MX_Yocto_Project_User's_Guide.pdf".

 

https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS 

  Also, please take a look at the following:

https://community.nxp.com/message/847773 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励
回复