change the i.MX6 cpu trip temperature (TEMP_CRITICAL),but cant reboot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

change the i.MX6 cpu trip temperature (TEMP_CRITICAL),but cant reboot

1,126 次查看
zhangzhencai
Contributor II

Dear all,

           I  change my TEMP_CRITICAL  by excuting the cmd " cat /sys/class/thermal/thermal_zone0/temp > /sys/class/thermal/thermal_zone0/trip_point_0_temp",then the board is died cant't reboot. There is no response when I press the reset button. Only  when i turn off power then turn on  the power ,the board  start running .

Serial port information:

  Chip is too hot, reboot!!!
   Watchdog re

Thanks.   

标签 (4)
0 项奖励
回复
0 回复数