Hello Champs,
I'm using OBDS(imx50_obds_release_v1_0.tar.gz) for i.MX50.
I built a bin file and when I try to write it to SD-card formatted in FAT32, I got this error:
cfimager-imx.exe -o 0 -f ./output/mx50/bin/diag-obds-mx50ref-rev3.bin -d e:
Error: error -23
What is error -23 ?
Best regards,
Nori Shinozaki
Please try to clear the SD using Linux command dd, as shown below (an example)
$ sudo dd if=/dev/zero of=/dev/sda bs=512 count=1000
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Yuri,
I didt that but I got the same result error -23.
I erased the SD-card with the "dd" command in Linux then, formatted in FAT32 in Windows.
You meant to use elftosb to write the bin file also in Linux?
No way to use cfimager-imx.exe?
Because my customer is using Cygwin and arm-none-eabi-gcc for Windows.
They can build the OBDS in Windows so they would like to write in Windows.
Best regards,
Nori Shinozaki