fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
ehci-mxc: Freescale On-Chip EHCI Host driver
xhci_hcd 0000:01:00.0: xHCI Host Controller
xhci_hcd 0000:01:00.0: new USB bus registered, assigned bus number 1
[XHCI FW Downloder] XHCI_FWDownLoadCheck
[XHCI FW Downloder] VenderID=1912, DeviceID=0014, Revision=0003
[XHCI FW Downloder] Device is 720201/202
[XHCI FW Downloder] --Revision 3
pci_bus 0000:01: firmware, attempted to load /lib/firmware/updates/3.14.28-1.0.0_ga+g91cf351/renesas/K2026090.mem, but failed with error 1
pci_bus 0000:01: firmware, attempted to load /lib/firmware/updates/renesas/K2026090.mem, but failed with error 1
pci_bus 0000:01: firmware, attempted to load /lib/firmware/3.14.28-1.0.0_ga+g91cf351/renesas/K2026090.mem, but failed with error 1
pci_bus 0000:01: firmware, attempted to load /lib/firmware/renesas/K2026090.mem, but failed with error 1
pci_bus 0000:01: Direct firmware load failed with error -2
Hi tom
firmware may fail to load due to kernel version incompatibility,
in general one can try to debug it using AN4553 Using Open Source Debugging
Tools for Linux on i.MX Processors
http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf
Also every device may require different firmware version, one can try to obtain updated
firmware for that particular device from renesas.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------