你好,我参考Manufacturing Tool V2 Linux or Android Firmware Development Guide V2文档,编译mfg frameware,使用mfgtool重新下载os到emmc,,但是此时出现了错误
mfgtool卡在了access boot partition 1
console信息:
UTP: executing "dd if=/dev/zero of=/dev/mmcblk0 bs=512 seek=1536 count=16"
请问:
1 是我编译的mfg frameware不对吗,还是要使用ltib来编译呢?
2 如果用ltib编译,应该参考哪个文档呢?
Solved! Go to Solution.
Hi hong wu,
Which BSP and board are you using?
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
另外:
1,我使用I.MX6DQSDL DDR3 Script Aid V0.10.xlsx文件生成的inc脚本,载入V2.60版本的DDR Test Tool,开始后tool停留在如下画面,无法得到DQS 等配置。应该如何解决
2,我的板子emmc从8G扩大至16G,mfgtool里面的mksdcard-android.sh文件是否需要修改,如果需要该,有没有说明文档可以参考!
你这个问题应该是 内存 参数或者 layout 有问题, 内存工作不稳定 导致.
谢谢,我让我们硬件工程师也检查一下。
android_jb4.3_1.0.0-ga
board is based on MX 6Quad SABRE-SD, just changed: DDR from 1G DDR2 to 2G ddr3; and emmc from 8G to 16G