boot config pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

boot config pins

2,175件の閲覧回数
sapirbuz
Contributor IV

Hi,

We are using MCU PN MIMXRT1051CVL5B.

The Boot will be through an external 8Mb serial NOR Flash using the NXP 3.3V FlexSPI port A secondary pins.

In our design, the only available config pins (that are used as configuration pins) are boot_mode[0] and boot_mode[1].

boot_cfc2[2:0] are GPIOs pins and can't be used as the boot configuration pins in our design because we planned to be in the boot from fuses mode and not the internal boot mode.

When we try to program the fuses by serial downloader, an error occurs saying that the external memory wasn't found.

How can we program the fuses without reading the boot_cfc2[2:0] and connecting to the external memory?

0 件の賞賛
返信
4 返答(返信)

2,158件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sapirbuz 

Could you please describe your question more detail and correct.

boot_cfc2[2:0] 

->> Do you meaning boot_cfg2[2:0]  ? And this is not pin, it is Fuse.

oot_mode[0] and boot_mode[1] are the boot pins.

 

BR

Alice

0 件の賞賛
返信

2,150件の閲覧回数
sapirbuz
Contributor IV

yes, boot_cfg[2:0]

0 件の賞賛
返信

2,145件の閲覧回数
sapirbuz
Contributor IV

We want to burn the fuses to define the secondary flash as a boot device, but we can't do it because we can't connect to the flashloader, and we can't connect to the flashloader because we can't burn the fuses.

please see the pictures below:

sapirbuz_0-1679412369368.png

 

sapirbuz_1-1679413107913.png

 

 

0 件の賞賛
返信

2,155件の閲覧回数
sapirbuz
Contributor IV

what data is missing? please elaborate

0 件の賞賛
返信