board detct on PC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

board detct on PC

1,690 Views
sachusanal
Contributor III

Hi ,

I need to detect my board on pc ,when I connected to my board to PC through USB otg port is not detecting , what shall I do for detecting ? I enabled HID support and USB support

Regards

Sachu

Labels (1)
0 Kudos
Reply
6 Replies

1,549 Views
aravinthkumarja
Senior Contributor II

Hi sachusanal​,

Your are using android(which version) or linux?

If you are using Android enable Below config:

CONFIG_USB_G_ANDROID

If linux,

CONFIG_USB_MASS_STORAGE

Try the above configuration it will work.

Regards,

Aravinth

0 Kudos
Reply

1,549 Views
sachusanal
Contributor III

Hai ,

Thanks for your reply .

I am using Linux Jethro build , I already configured  CONFIG_USB_MASS_STORAGE , let me know if any other configuration is required.?

Regards

Sachu

0 Kudos
Reply

1,549 Views
aravinthkumarja
Senior Contributor II

Hi sachusanal​,

Can you check in serial downloader mode the OTG is detected or not ??

Regards,

Aravinth

0 Kudos
Reply

1,549 Views
sachusanal
Contributor III

no , I need to HID communication between c# application and my board for software uopgrade.

when i give this configuration CONFIG_USB_MASS_STORAGE. it will be insterd as module. then modprobe g_mass_stoarge  command it will detected as mass storage. but I don't need to detect it as mass storage. it is detected for c# application and board communication.

please help me

0 Kudos
Reply

1,549 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sachu

using linux please check that USB_ID signal is high, also one can

check without OS setting pins BOOT_MODE[1:0]=01 Serial Downloader

during board power-up, please look at Chapter 8 System Boot i.MX6Q RM.

If that will not help please check Design Checklist recommendations in

i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,549 Views
sachusanal
Contributor III

Hai igor ,

thanks for your reply .

I hope hardware have no problem . I hope kernel configuration have some effect. could u please help me to find out that one?

Regards

Sachu

0 Kudos
Reply