bitbake fsl-image-qt5 error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

bitbake fsl-image-qt5 error

2,346 次查看
yenchou
Contributor III

HI All,

I use the Ubuntu 14.04 and the command:

DISTRO=fsl-imx-wayland MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-wayland-q

bitbake fsl-image-qt5

But it had a error:

/mnt/raid114/yen/L4.1.15/build-wayland-q/tmp/sysroots/x86_64-linux/usr/libexec/arm-poky-linux-gnueabi.gcc-cross-initial-arm/gcc/arm-poky-linux-gnueabi/5.2.0/ld:/mnt/raid114/yen/L4.1.15/build-wayland-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/glibc/2.22-r0/build-arm-poky-linux-gnueabi/shlib.lds:154: syntax error
| collect2: error: ld returned 1 exit status
| make[2]: *** [/mnt/raid114/yen/L4.1.15/build-wayland-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/glibc/2.22-r0/build-arm-poky-linux-gnueabi/libc.so] Error 1
| make[2]: *** Waiting for unfinished jobs....
| mv -f /mnt/raid114/yen/L4.1.15/build-wayland-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/glibc/2.22-r0/build-arm-poky-linux-gnueabi/elf/ld-linux-armhf.so.3.new /mnt/raid114/yen/L4.1.15/build-wayland-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/glibc/2.22-r0/build-arm-poky-linux-gnueabi/elf/ld-linux-armhf.so.3
| make[2]: Leaving directory `/mnt/raid114/yen/L4.1.15/build-wayland-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/glibc/2.22-r0/git/elf'
| make[1]: *** [elf/subdir_lib] Error 2
| make[1]: Leaving directory `/mnt/raid114/yen/L4.1.15/build-wayland-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/glibc/2.22-r0/git'
| make: *** [all] Error 2
| WARNING: exit code 1 from a shell command.
| ERROR: oe_runmake failed
| ERROR: Function failed: do_compile (log file is located at /mnt/raid114/yen/L4.1.15/build-wayland-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/glibc/2.22-r0/temp/log.do_compile.16758)
ERROR: Task 725 (/mnt/raid114/yen/L4.1.15/sources/poky/meta/recipes-core/glibc/glibc_2.22.bb, do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2052 tasks of which 5 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:

Summary: 1 task failed:
/mnt/raid114/yen/L4.1.15/sources/poky/meta/recipes-core/glibc/glibc_2.22.bb, do_compile
Summary: There were 2 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

How could I solve the problem?

Have a great day,

Yen

标签 (1)
标记 (1)
0 项奖励
回复
4 回复数

1,679 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please try the recent NXP BSP. Follow recommendations of "i.MX_Yocto_Project_User's_Guide.pdf".

https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS 

Summary page:

i.MX Software|NXP 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,679 次查看
yenchou
Contributor III

Hi,Yuri

Thank you for your answer,though it dose not solve my problem.

Have a great day,

Yen

0 项奖励
回复

1,679 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  I just managed to built   fsl-image-qt5, using Your commands, 
under Debian 8. 

Regards,

Yuri.

0 项奖励
回复

1,679 次查看
yenchou
Contributor III

Hi,Yuri

Thank you for your kind help,I used commands in the ubuntu14.04  virtual machine was normal.

But it producted error in the ubuntu14.04 server.

0 项奖励
回复