I just download the Adeneo android 4.1 which is base on FSL r10.3 patch for QSB.
I set the boot arg as below:
setenv hdmi 'setenv bootargs ${bootargs} init=/init androidboot.console=ttymxc0 video=mxcdi0fb:RGB24,1920x1080M@60 hdmi di0_primary gpu_memory=256M'
but when I try to play a video, I got the kernel fatal error, the accessory is the error-log
It seems a DMA error.
I wanna know whether the QSB can play video on Adeneo 4.1 system?
I can play video on Adeneo 4.0 system before.
Thanks advance!
Correctly, thank you very very much ! Leon
It fix the issue now!
That kernel seems broken in one respect, this is a known issue with a known fix.
It needs this fix (or better the Freescale fix patch set for 11.09, as it solves the problem more reliably).
http://imxcommunity.org/group/imx53quickstartboard/forum/topics/playing-1080p-video-on-a-1080p-panel
Regards,
Leon.